Other Parts Discussed in Thread: SYSBIOS
Greetings,
I was hoping that someone could provide me some direction as to how I might go about trouble-shooting the following instruction fetch exception. The application is a modification of the System Analyzer Tutorial 4C.
- [C66xx_2] A0=0x0 A1=0x0
- [C66xx_2] A2=0x0 A3=0x0
- [C66xx_2] A4=0x0 A5=0x1
- [C66xx_2] A6=0x193 A7=0x0
- [C66xx_2] A8=0xc0006ec A9=0x1
- [C66xx_2] A10=0xfffffffc A11=0x2
- [C66xx_2] A12=0x0 A13=0xc0000b8
- [C66xx_2] A14=0xc0006ec A15=0xc195830
- [C66xx_2] A16=0xc205780 A17=0x10
- [C66xx_2] A18=0x806780 A19=0x30
- [C66xx_2] A20=0x6c A21=0x4c
- [C66xx_2] A22=0x40100581 A23=0xb040
- [C66xx_2] A24=0x420880 A25=0x8031000c
- [C66xx_2] A26=0x84605 A27=0x60800006
- [C66xx_2] A28=0x20000 A29=0x0
- [C66xx_2] A30=0xc1932dc A31=0x0
- [C66xx_2] B0=0x1 B1=0x0
- [C66xx_2] B2=0x0 B3=0xc323e24
- [C66xx_2] B4=0x2 B5=0xc1930a8
- [C66xx_2] B6=0xf580010 B7=0xc192af0
- [C66xx_2] B8=0x0 B9=0x0
- [C66xx_2] B10=0x90 B11=0x1
- [C66xx_2] B12=0x2 B13=0xc37b1e0
- [C66xx_2] B14=0x806f98 B15=0x8068c8
- [C66xx_2] B16=0x8068b8 B17=0x0
- [C66xx_2] B18=0xc0004f0 B19=0xc
- [C66xx_2] B20=0x69 B21=0x3
- [C66xx_2] B22=0x3 B23=0x0
- [C66xx_2] B24=0x9c002cc4 B25=0xc4002200
- [C66xx_2] B26=0x304482 B27=0x22400302
- [C66xx_2] B28=0x420a0900 B29=0x8005202a
- [C66xx_2] B30=0x0 B31=0x1
- [C66xx_2] NTSR=0x1000c
- [C66xx_2] ITSR=0x0
- [C66xx_2] IRP=0x0
- [C66xx_2] SSR=0x0
- [C66xx_2] AMR=0x0
- [C66xx_2] RILC=0x0
- [C66xx_2] ILC=0x0
- [C66xx_2] Exception at 0x0
- [C66xx_2] EFR=0x2 NRP=0x0
- [C66xx_2] Internal exception: IERR=0x1
- [C66xx_2] Instruction fetch exception
- [C66xx_2] ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x00000000, sp = 0x008068c8.
- [C66xx_2] xdc.runtime.Error.raise: terminating execution
Basically, which tools in CCS5.1 do I use to trace the problem to its root cause? I there a good tutorial on how debug such a problem?