This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100v1 with CCS 5.1 on Linux?



If I set up a target configuration (.ccxml) file for the TI XDS100v1 emulator on CCS 5.1 under Linux, and click the "Test Connection" button, I get the following error:

Cannot run program "/opt/ti/ccsv5/ccs_base/common/uscif/dbgjtag.exe": java.io.IOException: error=2, No such file or directory

That is easy enough to work around by editing /opt/ti/ccsv5/ccs_base/common/targetdb/connections/TIXDS100usb_Connection.xml and removing the extra .exe.  When I try to test the connection with that change, I get the following error:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


  The [-f] option was used, but the board config
  file was not found or lacked read permission.
  Its name was: '"/home/mpoole/.TI/3205019477/0/0/BrdDat/testBoard.dat"'.


[End]

It looks like there is an extra level of quoting in the expanded file name.  Is there a way to work around that, short of writing a shell script to run as the diagnostic command?