Part Number: CODECOMPOSER
Tool/software:
Hi.
When I try to import a project designed with CCSv7 into CCSv8 or CCSv12, I get the message "Import failed for project 'DSP' because its meta-data can't be interpreted. Please contact support." and I can't import it.
('DSP' is the project folder name)
CCSv7.4.0.00015 -> CCSv8.3.1.00004
CCSv7.4.0.00015 -> CCSv12.0.0.00009
The same message appears in either case.
Question:
Does the meta-data format change significantly depending on the version?
Are there any restrictions on the versions that can successfully load CCSv7.4.0.00015 meta-data?
Thanks.