Part Number: CODECOMPOSER
Tool/software:
Hi,
I would like to test the communication between controllers (both F280039C launchpads). To do so, I opened 2 instances of CCS (20.1.1) and launched one debug session in each instance. However, I get an error for the second instance :

The error is always on the debug session that is launched second. It is not board dependent, nor is it CCS instance dependent.
Is it possible to have 2 debug sessions, 1 for each side of the communication, on the same computer ? Or do I absolutely need a second computer to do so ?
Thanks in advance,
Best regards,
Adrien