This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: MSPM0G3107 writing nonmain section via XDS Debugger

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: LP-MSPM0G3507, UNIFLASH

Tool/software:

Hi 

since i currently have issues with my jlink probe i have switched to the XDS programmer on the LP-MSPM0G3507 connected to my external target. 

I have a binary that contains non default contents for the Nonmain section; while with the jlink probe it works seemlessly to erase the nonmain section and then overwrite it when starting a debug session with the XDS probe this is not the case i also can not seem to find a setting to change that. Instead i am getting 

The same is true when attempting to "just production flash" using uniflash -- where that same error would come up but there atleast a setting is available to do a mass erase of multiple sections (nonmain included) and then do the programming in another step afterwards

It strikes me as odd that (while the jlink probe is not perfect) the 3rd party (jlink) probe works more seemlessly than your own 1st party solution...