This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot open existing project in place (v. 5.1.0.09000)

I am trying to open existing project with Code Composer 5.1.0.09000.

File - Import - Code Composer Studio - Existing CCs/CCE Eclipse Projects - Next. Directory: C:\StellarisWare\boards\rdk-s2e\ser2enet. Once I select ser2enet project in the Discovered Projects window, "Copy projects into workspace" checkbox is automatically checked and disabled. As result, the project is copied to the workspace directory and cannot be compiled because of relative include paths.

In Code Composer 4.2.4 it is possible to open projects in place, without copying them into workspace directory. How can I do the same in new version?