Part Number: CODECOMPOSER
Other Parts Discussed in Thread: AM263P4, ENERGYTRACE
Tool/software:
Hello,
Am using Eclipse 12.8.1 with Hardware Trace Analyzer Function Profiler with AM263P4 (400MHz).
In my application there is a function called every 1ms by FreeRTOS. The function is called Xcp_Test_IncCounter1ms().
The Trace Analyzer manual says: "The Per Call view provides a list of all function calls that occurred with the time (in cycles) when the function was entered and exited".
My function is called twice in the example below:

The first call is at 855 cycles and the second at 143244 cycles a difference of 142389.
My problem is the meaning of "cycles". I thought that this would be the number of CPU cycles but that t doesn't seem to match the expected numbers.
1ms / 142389 = 7.02ns (142.4MHz)
<Q>
Why does 1 cycle = 7ns please? Put another why doesn't 1 cycle = 2.5ns (400MHz)?
Thank you.