Hi,
I'm encountering the CCS5 IDE performance problems while opening, creating, debugging and editing projects.
For debugging I use XDS100v2 emulator for OMAP L-138, C6748 Core.
Sometimes the IDE doesn't run to main on program load despite the appropriate option is selected.
Generally, the IDE is running in a very unsmooth way, stuck while opening project, stuck while moving from editor perspective to the debug mode.
I'm running it on WIndows XP. I have tested it on two pc's : the same result.
How can I improve the performance? Is there any update or patch for the IDE for that purposes?
Anatoly.