Other Parts Discussed in Thread: CCSTUDIO
I am running CCS v5.1.09000 under Ubuntu 10.04. The target I'm using is the C6472 EVM.
lsusb recognizes the device.
The Bh560v2Config utility passes fine, so is seems that the device drivers and Blackhawk CCS files are installed properly.
But, when attempting to connect to the device, CCS reports the following error:
"ICEPICK_C_0: Error initializing emulator: (Error -2085 @ 0x0) Internal error: Missing or corrupt application file. Restart the application. If error persists, please report the error. (Emulation package 5.0.520.0) "
I've tried re-installing CCS, I've tried this in v. 5.0.3 and on a different Ubuntu machine and the result is always the same.
I am able to use an SD XDS510 on the same setup with no issues.