Part Number: CODECOMPOSER
Tool/software:
I've installed the latest Mac version I could find - 20.1.1.8__1.7.1 on a Macbook M2
When I try and build one of the example projects it fails with:
ImportError: dlopen(/Library/Frameworks/Python.framework/Versions/3.11/lib/python3.11/site-packages/_cffi_backend.cpython-311-darwin.so, 0x0002): tried: '/Library/Frameworks/Python.framework/Versions/3.11/lib/python3.11/site-packages/_cffi_backend.cpython-311-darwin.so' (mach-o file, but is an incompatible architecture (have 'arm64', need 'x86_64')), '/System/Volumes/Preboot/Cryptexes/OS/Library/Frameworks/Python.framework/Versions/3.11/lib/python3.11/site-packages/_cffi_backend.cpython-311-darwin.so' (no such file), '/Library/Frameworks/Python.framework/Versions/3.11/lib/python3.11/site-packages/_cffi_backend.cpython-311-darwin.so' (mach-o file, but is an incompatible architecture (have 'arm64', need 'x86_64'))
[112]thread '<unnamed>' panicked at 'Python API call failed', /Users/runner/.cargo/registry/src/index.crates.io-6f17d22bba15001f/pyo3-0.18.3/src/err/mod.rs:790:5
No errors or warning on installation
Are there any recommended ways to get this working with the build needing an x86_64 library on an ARM64 machine?
Regards
Neil