Part Number: CODECOMPOSER
Tool/software:
Hello TI Community,
I am experiencing a persistent issue with Code Composer Studio (CCS) version 12.8.1 on Windows. Whenever I open Resource Explorer, the panel continuously refreshes and displays a “Task Updated” overlay, making it impossible to browse or import any resources or example projects. The overlay never clears, and Resource Explorer remains unusable. If I somehow get to the project and try to import, the entire application becomes unresponsive. I have to force-quit CCS via Task Manager.
Troubleshooting Steps Taken:
-
Cleared CCS and browser caches
-
Restarted CCS and the computer
-
Checked network and proxy settings (direct internet connection, no proxy)
-
Uninstalled and reinstalled CCS 12.8.1
Despite these efforts, the issue persists. I have also confirmed that my internet connection is stable.
Questions:
-
Is this a known issue in CCS 12.8.1?
-
Are there any workarounds or patches available?
Any advice or insights would be greatly appreciated. Thank you!
System Details:
-
CCS version: 12.8.1
-
OS: Windows 11 (64-bit)
-
Internet: Direct connection, no proxy