Hi
My CCSv4 somehow screwed up its editor such that I could not close tabs or access the additional files by clicking on the tab expansion. After I rebooted, tried different workspaces, I decided to uninstall CCSv4 and start a new. I used windows Add/Remove tool to delete CCSv4.
Unfortunately, when I try to install, I get the error
"You are trying to overinstall CCS v4.0.0.0 with v4.2.4.00033 in same directory. This is not allowed. Please choose a different folder and try again"
I checked my "C:\Program Files\Texas Instruments" folder and I only have ccsv5. Could it be that ccsv4 thinks ccsv5 is a ccsv4 version? (its crazy, but I'm willing to believe anything now!)
Furthermore, I don't think I ever installed CCSv4.0.0.0!!!!
This is a show stopper. I have to get CCSv4 installed to get a product build done!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
Cheers