hi,
My USB FET debugger is not working with CCS but it is working with IAR . the Mode (Red) led is not blinking while am connecting USB cable , power led(green
) is glowing. pls help me to debug.
-pratheep
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
My USB FET debugger is not working with CCS but it is working with IAR . the Mode (Red) led is not blinking while am connecting USB cable , power led(green
) is glowing. pls help me to debug.
-pratheep
Hello Pratheep,
this is likely due to different dll versions. What version of dll at the two using? What version of CCS and IAR are you using? Does you FET show up as a CDC Class USB device in the device manager?
Have a look at this wiki topic as well.
http://processors.wiki.ti.com/index.php/MSP_Debug_Stack
Please keep us posted and we can go from there.
Best Regards,
Lisa
Hi,
My MCU is MSP430F2619, also i am using the target board and the USBFET430UIF
In TARGET BOARD : whenever i burn a program(LED blink) and remove the power supply, obviously LED stops blinking, BUT on giving power supply the next time, the LED starts blinking automatically
Which means the program resumes when the MCU gets power.
How do i erase all memory (previous code) before i dump my new program. For now i just punch the debug button and just wait for the program to get loaded. I get the "MCU is busy" error, but i punch the retry button a couple of times and it works.
BUT, i want to know how to erase all memory (previous code) before i dump my new program.
please help
Thanks.
Hello,
see the attached screenshot to get to the memory options. Also note I would very highly recommend upgrading to the latest production version of CCS which is 4.2.4. The screenshot starts from Project->Properties.
Please keep us posted.
Best Regards,
Lisa

Hi Lisa,
I Am using CCSv4 and IAR-v6. after am fusing a code from IARv6 the FET is not communicating with CCS. In device manager it showing CDC. i have downloaded the CDC driver but it is not communicating with CCS still.
-pratheep
Hello Lisa,
Thanks for the quick reply, i have tried selecting the Erase main and info memory option, but my problem persists.
Let me take you through the steps i take to load a program.
Step 1: CCS project > source file > LED blink program > punch Debug
Step 2: punch the green play button > LED blinks
Step 3: Terminate the program (red box button)
Step 4: change the source file (copy-paste the dac program) > save it
Step 5: Punch the debug button.
NOW i get an error "Error initializing emulator: MSP-FET430UIF is already in use."
Step 6: I punch the retry button a couple of times, the program eventually gets loaded into the MCU, program runs fine.
Now, how do i erase or stop the execution of previous code before i load the new code??
Hi Pratheep,
what you are seeing is caused by the dll version. Please see this wiki. If you wish to use both the latest IAR and CCSv4 you will have to upgrade and downgrade your FET each time to go in between the two tools. Otherwise you will have to migrate to or install CCSv5.1 which will then have both IAR and CCS using the same dll and resolve your issue.
http://processors.wiki.ti.com/index.php/MSP_Debug_Stack
If you can not install or migrate to v5.1 please let me know. I can send you the upgrade/downgrade utility offline.
BEst Regards,
Lisa
Hi Janmay,
Have a look under Project->properties->CCS Debug->Target. Here you will find the options on the behaviour to do with debug. Ie halting the target, automatic loading, etc.
I have attached a screenshot for you as well.
Please keep us informed.
Best Regards,
LIsa
Hi Janmay,
very glad to hear and a happy new year to you as well.
Best Regards,
Lisa