This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS470 tool chain version 4.6.3 throws error while building the DM816x codebase

Hi,

I am getting the unhandled exception while building the codebase using TMS470 tool chain version 4.6.3. Everytime, the error occurs at different files while building.

I tried with both CCS 4.2.0 version IDE and command window.

The tool chain was working fine previously, but suddenly this issue started.

I got struck because of this issue. Please help me to resolve this issue.

Thanks in Advance.

Software details:

OS : Windows XP

CG tools: TMS470 V 4.6.3

CCS : 4.2.0

Regards,

Dhana.

 

 

  • Dhana,

    I suspect you are running into a known issue that we fixed a while ago. The bug # is SDSCM00036371 and caused the shell to crash randomly at different parts of the build. You may look at the details/status of the bug using the  SDOWP link in imy signature and entering the above bug #.

    This bug should be fixed in v4.6.4 and higher of the TMS470 cgtools, so please give the newer version a try and let us know if the problem persists.
    The latest release on the 4.6.x stream is 4.6.6. You can update to this version via CCS Update Manager.
    http://processors.wiki.ti.com/index.php/Compiler_Releases