This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to get target ip address of AM37xx board sitara processor

after giving command 

root@dm3730-am3715-evm:~# ifup eth0

it showed already configured

root@dm3730-am3715-evm:~#ifconfig

i got only local ip address

i didn't got target evm address

how to find that or is there possible to set any ip address 

  • I think you might posting to the wrong forum. Your question might fit better in the Embedded->Linux sub-forum. Some other details might be required. Are you using static addresses or DHCP? What are your bootargs? What is the contents of your /etc/network/interfaces file? Is the network actually working? Can you ping or tftp?

  • yes,it is DHCP.

    BOOTARGS are 

    console=ttyS0,115200n8 root=/dev/mmcblk0p2 rw ip=192.168.15.99 mem=99 mpurate=1000  omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp=lcd rootwait


     

  • Your bootargs assign a static address. For DHCP, use ip=dhcp. Does your bootup log messages show the network being configured? It's a few lines starting with "IP-Config: Complete:".

    You can use the ifconfig to setup the network after boot. If it is already configured, first issue a ifdown. You might have to manually start a DHCP client. That varies with different Linux versions. I normally let the bootup setup the network.

  • karthik ,

    karthik tata said:

    i didn't got target evm address

    how to find that or is there possible to set any ip address 

    to get the IP address of the target, try:

    > ifconfig | grep inet

    to set an ipaddress, try:

    > ifconfig eth0 <ip address>

    thanks

    ki