This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Loading Program is too slow through XDS510USB-PLUS via JSC

Other Parts Discussed in Thread: OMAP-L138

I am using XDS510PLUS-USB and OMAP-L138 experimental board. My pc is Windows7 64bit.

When I select Spectrum Digital XDS510USB at target setup(this is wrong configuration), time of loading program to SDRAM is within 10 sec.

But When I select XDS510USB-PLUS via JSC, time of loading program to SDRAM is over 2 minuts !!

Could anyone help me ?

  • Hi Shigeo,

    The XDS510 is a higher speed and preformance emulator, so it is expected it will perform better, faster and have a few more features.  Please see the following wiki topics I hope will help.

    http://processors.wiki.ti.com/index.php/XDS510

    http://processors.wiki.ti.com/index.php/XDS100

    http://processors.wiki.ti.com/index.php/Category:Emulation

    Please keep us informed.

    Best Regards,
    LIsa