This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: "fatal error - cygheap base mismatch detected" when building an XDC project

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TM4C1294NCPDT

Tool/software:

I get the following error when trying to build an existing project on CCS20:

[11]Building file: "../myfile.cfg"
[12]Invoking: XDCtools
[13]"C:/ti/xdctools_3_32_00_06_core/xs" --xdcpath="C:/ti/tirtos_tivac_2_10_01_38/packages;C:/ti/tirtos_tivac_2_10_01_38/products/bios_6_41_00_26/packages;C:/ti/tirtos_tivac_2_10_01_38/products/ndk_2_24_01_18/packages;C:/ti/tirtos_tivac_2_10_01_38/products/uia_2_00_02_39/packages;C:/Users/dant1/git/cmdl1-er-firmware/CMDL1-ER_TIRTOS;C:/ti/ccs2020/ccs/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -p ti.platforms.tiva:TM4C1294NCPDT -r debug -c "C:/ti/ti-cgt-arm_20.2.7.LTS" --compileOptions "-mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O3 --include_path=\"C:/ti/ti-cgt-arm_20.2.7.LTS/include\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/CMDL1-ER_TIRTOS\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party/lwip-1.4.1/src/include\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party/lwip-1.4.1/src/include/ipv4\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party/lwip-1.4.1/apps\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party/lwip-1.4.1/ports/tiva-tm4c129/include\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party/Cgipp\" --include_path=\"C:/Users/dant1/git/cmdl1-er-firmware/common/third_party\" --include_path=\"C:/ti/tirtos_tivac_2_10_01_38/products/TivaWare_C_Series-2.1.0.12573c\" --include_path=\"C:/ti/tirtos_tivac_2_10_01_38/products/ndk_2_24_01_18/packages/ti/ndk/inc\" --include_path=\"C:/ti/tirtos_tivac_2_10_01_38/products/ndk_2_24_01_18/packages/ti/ndk/inc/bsd\" --include_path=\"common/System/include\" --include_path=\"C:/ti/ti-cgt-arm_20.2.7.LTS/include/libcxx\" --preinclude=\"stdint.h\" --define=ccs=\"ccs\" --define=CMDL1R --define=TI_RTOS --define=SYSTEM_CLOCK_FREQ=120000000 --define=PART_TM4C1294NCPDT --define=TARGET_IS_TM4C129_RA2 --define=ccs --define=TIVAWARE -g --c11 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi " "../CMDL1-ER.cfg"
[14] 1 [main] ? (43228) C:\ti\xdctools_3_32_00_06_core\bin\sh.exe: *** fatal error - cygheap base mismatch detected - 0xEC88E0/0xDF88E0.
[15]This problem is probably due to using incompatible versions of the cygwin DLL.
[16]Search for cygwin1.dll using the Windows Start->Find/Search facility
[17]and delete all but the most recent version. The most recent version *should*
[18]reside in x:\cygwin\bin, where 'x' is the drive on which you have
[19]installed the cygwin distribution. Rebooting is also suggested if you
[20]are unable to find another cygwin DLL.

The cygwin1.dll in CCS20 is incompatible with the cygwin.1.dll that ships with xdctools_3_32_00_06_core. I installed them both at the same time.