Hello,
I have an exception being thrown and I am attempting to debug it using trace. I am running on an C6472 demo board, and using the embedded trace buffer. I have the two trace break points as described in the wiki, but whenever I actually run, the trace log has very items in the listing. It has the usual begin and end, and it also usually has one more which says something about an incomplete packet or something or other. I was under the impression that even though the ETB is a circular buffer, I should still be able to see the last X instructions?
I am running CCSv5 with an XDS510 jtag pod
Thanks