Part Number: CODECOMPOSER
Tool/software:
Hello,
I want to maintain a single SysCfg file for two very similar projects but one project has fewer source files than the other.
With the following linker script:
GROUP : {
FAST_FUNCTIONS : {
file_a.o(.text)
file_b.o(.text)
} align(8)
} > R5F_TCMA
file_a.c and file_b.c exist in Project A but not in Project B.
When Project B is linked I get an error:
I don't see why this should be a fatal error. So what if these files don't exist?
- Is there a different syntax that avoid this error please?
- If not, is there any way to make this error a warning instead please?
I want it to continue to make the build artefacts even if no file matches the pattern.
Thank you.