This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.1 Licensing Problem



Hi,

I have a  TMDSCCS-MCUN01-v4.0.

I already activated received lisense file.

Recently I installed CCSv5.1.

And I installed license TMDSCCS-MCUN01-v4.0.lic.

But CCSv5.1 is unlicensed.

CCSv5.1 can use TMDSCCS-MCUN01-v4.0 license file?

My CCS version is v5.1.00.09000

Below image is location of license.

  • Hi Remony,

    unfortunately your v4 license will not work with v5.1.   You have three options

    - see if you are eligible for an upgrade (if you have a current subscription then you should be).  You should see this in www.ti.com/myregisteredsoftware

    - buy a v5 license

    - use one of the free license options (eg v5.1 is basically free to use with the XDS100 emulator).


    This wiki should also be helpful.  Please keep us informed.

    http://processors.wiki.ti.com/index.php/Licensing_-_CCS

    Best Regards,

    Lisa