This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS470 Toolchain configuration.



Hi,

I'm new to Linux development and have just installed the SDK "AM3517SDK 05_03_02_00" according to the installation guide.

My target platform is the Zoom AM3517EVM from Logic PD.
I have the bootloader and the 2.6.37 kernel running on the target platform. (Recompiled from sources.)

I noticed that CCS is now using the TMS470 toolchain instead of the Code Sourcery toolchain which I have previousley used with CCS 5.0.1.

When I create a new CCS Project with default settings I am unable to succesfully build a hello world application using the new setup.

The source for the program is simple:

#include <stdio.h>

/*
 * hello.c
 */
void main(void) {
    printf("Hello World!\n");
}

The output from the build process is:

**** Build of configuration Debug for project hello_world ****

/opt/ti/ccsv5/utils/bin/gmake -k all
Building file: ../hello.c
Invoking: TMS470 Compiler
"/opt/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7A8 -g --include_path="/opt/ti/ccsv5/tools/compiler/tms470/include" --diag_warning=225 --display_error_number --abi=eabi --code_state=32 --preproc_with_compile --preproc_dependency="hello.pp"  "../hello.c"
Finished building: ../hello.c
 
Building target: hello_world.out
Invoking: TMS470 Linker
"/opt/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7A8 -g --diag_warning=225 --display_error_number --abi=eabi --code_state=32 -z -m"hello_world.map" --warn_sections -i"/opt/ti/ccsv5/tools/compiler/tms470/lib" -i"/opt/ti/ccsv5/tools/compiler/tms470/include" --reread_libs --rom_model --be32 -o "hello_world.out"  "./hello.obj" -l"libc.a"
<Linking>
warning #10247-D: creating output section ".sysmem" without a SECTIONS
   specification
warning #10210-D: creating ".stack" section with default size of 0x800; use the
   -stack option to change the default size
warning #10210-D: creating ".sysmem" section with default size of 0x800; use
   the -heap option to change the default size
Finished building target: hello_world.out

**** Build Finished ****

When I run the hello_world.out on the target board i get the error " /usr/bin/hello_world.out: line 1: syntax error: word unexpected (expecting ")") ", which to me suggest that the file is not recognized as an executable.

If I change the Device Endianness from "be32" to "little" and rebuild and rerun on the target I get the message "Killed".

I must be missing something obvious but I just don't see it.

Does anyone have a suggestion?

Best regards,
Brian.