This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM263P: It gets stuck when I try to build the example

Part Number: LP-AM263P

Tool/software:

Hi team,

I'm trying to flash the example of AM263P SDK. The SDK is "mcu_plus_sdk_am263px_11_00_00_19".

Also example is "get: "canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang".

But when I try to build project, Building process is stuck during building target.

Please see my output log. this is the last log that when it stuck. it seems python command is not working. Could you please review it? I checked the python requirements as explained here and it's fine : https://software-dl.ti.com/mcu-plus-sdk/esd/AM263PX/11_00_00_19/exports/docs/api_guide_am263px/SDK_DOWNLOAD_PAGE.html#autotoc_md13


[111]C:/ti/ccs2030/ccs/utils/bin/gmake -C C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang -f makefile_ccs_bootimage_gen OUTNAME=canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang PROFILE=Release MCU_PLUS_SDK_PATH=C:/ti/mcu_plus_sdk_am263px_11_00_00_19 CG_TOOL_ROOT=C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS CCS_INSTALL_DIR=C:\ti\ccs2030\ccs\ CCS_IDE_MODE=desktop DEVICE=am263px
[112] Boot multi-core ELF image: am263px:r5fss0-0:nortos:ti-arm-clang C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.mcelf ...
[113]python C:/ti/mcu_plus_sdk_am263px_11_00_00_19/tools/boot/multicore-elf/genimage.py --core-img=0:Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out --output=C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.mcelf --merge-segments=true --tolerance-limit=0 --ignore-context=false --xip=0x60000000:0x68000000 --xlat=none --max-segment-size=8192

Thank you.

Best Regards,

Donnie Kim

  • Hi Donnie,

    Please attach the full error log,The error log attached does not have error code mentioned.

  • Hi Nilabh,

    I attached the full log. But please note that there is no error or absort. It is just keep stuck over 20minute in same step.

    If you need any details, please let me know.

    Thank you for support.

    [13]"C:\\ti\\ccs2030\\ccs\\utils\\bin\\gmake" -k -j 14 all -O
    
    [14]Building file: "../example.syscfg"
    [15]Invoking: SysConfig
    [16]"C:/ti/ccs2030/ccs/utils/sysconfig_1.25.0/sysconfig_cli.bat" --script "C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/example.syscfg" -o "syscfg" -s "C:/ti/mcu_plus_sdk_am263px_11_00_00_19/.metadata/product.json" -p "ZCZ_C" -r "AM263P4" --context "r5fss0-0" --compiler ticlang
    [17]Running script...
    [18]Validating...
    [19]info: CONFIG_MPU_REGION3(/kernel/dpl/mpu_armv7) attributes: Some memory region(s) within this range is Shared among cores.
    [20]info: /kernel/dpl/debug_log uartLog.baudRate: Actual Baudrate Possible: 115385 (0 % error)
    [21]Generating Code (example.syscfg)...
    [22]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_dpl_config.c...
    [23]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_dpl_config.h...
    [24]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_drivers_config.c...
    [25]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_drivers_config.h...
    [26]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_drivers_open_close.c...
    [27]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_drivers_open_close.h...
    [28]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_pinmux_config.c...
    [29]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\pinmux.csv...
    [30]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_power_clock_config.c...
    [31]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_board_config.c...
    [32]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_board_config.h...
    [33]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_board_open_close.c...
    [34]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_board_open_close.h...
    [35]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_config.c...
    [36]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_config.h...
    [37]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_open_close.c...
    [38]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_open_close.h...
    [39]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_soc.c...
    [40]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_lwipif.c...
    [41]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_enet_lwipif.h...
    [42]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\linker.cmd...
    [43]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\linker_defines.h...
    [44]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_sdl_config.c...
    [45]Writing C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\syscfg\ti_sdl_config.h...
    [46]Finished building: "../example.syscfg"
    
    [47]Building file: "../canfd_external_read_write.c"
    [48]Invoking: Arm Compiler
    [49]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"canfd_external_read_write.d_raw" -MT"canfd_external_read_write.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"canfd_external_read_write.o" "../canfd_external_read_write.c"
    [50]Finished building: "../canfd_external_read_write.c"
    
    [51]Building file: "../canfd_transceiver.c"
    [52]Invoking: Arm Compiler
    [53]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"canfd_transceiver.d_raw" -MT"canfd_transceiver.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"canfd_transceiver.o" "../canfd_transceiver.c"
    [54]Finished building: "../canfd_transceiver.c"
    
    [55]Building file: "syscfg/ti_dpl_config.c"
    [56]Invoking: Arm Compiler
    [57]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_dpl_config.d_raw" -MT"syscfg/ti_dpl_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_dpl_config.o" "syscfg/ti_dpl_config.c"
    [58]Finished building: "syscfg/ti_dpl_config.c"
    
    [59]Building file: "syscfg/ti_drivers_config.c"
    [60]Invoking: Arm Compiler
    [61]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_drivers_config.d_raw" -MT"syscfg/ti_drivers_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_drivers_config.o" "syscfg/ti_drivers_config.c"
    [62]Finished building: "syscfg/ti_drivers_config.c"
    
    [63]Building file: "syscfg/ti_drivers_open_close.c"
    [64]Invoking: Arm Compiler
    [65]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_drivers_open_close.d_raw" -MT"syscfg/ti_drivers_open_close.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_drivers_open_close.o" "syscfg/ti_drivers_open_close.c"
    [66]Finished building: "syscfg/ti_drivers_open_close.c"
    
    [67]Building file: "syscfg/ti_pinmux_config.c"
    [68]Invoking: Arm Compiler
    [69]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_pinmux_config.d_raw" -MT"syscfg/ti_pinmux_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_pinmux_config.o" "syscfg/ti_pinmux_config.c"
    [70]Finished building: "syscfg/ti_pinmux_config.c"
    
    [71]Building file: "syscfg/ti_power_clock_config.c"
    [72]Invoking: Arm Compiler
    [73]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_power_clock_config.d_raw" -MT"syscfg/ti_power_clock_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_power_clock_config.o" "syscfg/ti_power_clock_config.c"
    [74]Finished building: "syscfg/ti_power_clock_config.c"
    
    [75]Building file: "syscfg/ti_board_config.c"
    [76]Invoking: Arm Compiler
    [77]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_board_config.d_raw" -MT"syscfg/ti_board_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_board_config.o" "syscfg/ti_board_config.c"
    [78]Finished building: "syscfg/ti_board_config.c"
    
    [79]Building file: "syscfg/ti_board_open_close.c"
    [80]Invoking: Arm Compiler
    [81]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_board_open_close.d_raw" -MT"syscfg/ti_board_open_close.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_board_open_close.o" "syscfg/ti_board_open_close.c"
    [82]Finished building: "syscfg/ti_board_open_close.c"
    
    [83]Building file: "syscfg/ti_enet_config.c"
    [84]Invoking: Arm Compiler
    [85]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_enet_config.d_raw" -MT"syscfg/ti_enet_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_enet_config.o" "syscfg/ti_enet_config.c"
    [86]Finished building: "syscfg/ti_enet_config.c"
    
    [87]Building file: "syscfg/ti_enet_open_close.c"
    [88]Invoking: Arm Compiler
    [89]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_enet_open_close.d_raw" -MT"syscfg/ti_enet_open_close.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_enet_open_close.o" "syscfg/ti_enet_open_close.c"
    [90]Finished building: "syscfg/ti_enet_open_close.c"
    
    [91]Building file: "syscfg/ti_enet_soc.c"
    [92]Invoking: Arm Compiler
    [93]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_enet_soc.d_raw" -MT"syscfg/ti_enet_soc.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_enet_soc.o" "syscfg/ti_enet_soc.c"
    [94]Finished building: "syscfg/ti_enet_soc.c"
    
    [95]Building file: "syscfg/ti_enet_lwipif.c"
    [96]Invoking: Arm Compiler
    [97]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_enet_lwipif.d_raw" -MT"syscfg/ti_enet_lwipif.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_enet_lwipif.o" "syscfg/ti_enet_lwipif.c"
    [98]Finished building: "syscfg/ti_enet_lwipif.c"
    
    [99]Building file: "syscfg/ti_sdl_config.c"
    [100]Invoking: Arm Compiler
    [101]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_sdl_config.d_raw" -MT"syscfg/ti_sdl_config.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"syscfg/ti_sdl_config.o" "syscfg/ti_sdl_config.c"
    [102]Finished building: "syscfg/ti_sdl_config.c"
    
    [103]Building file: "../main.c"
    [104]Invoking: Arm Compiler
    [105]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -I"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source" -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"main.d_raw" -MT"main.o" -I"C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/syscfg"   -o"main.o" "../main.c"
    [106]Finished building: "../main.c"
    
    [107]Building target: "canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out"
    [108]Invoking: Arm Linker
    [109]"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/bin/tiarmclang.exe" -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -Os -DSOC_AM263PX -DOS_NORTOS -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wl,-m"canfd_external_read_write.Release.map" -Wl,-i"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source/kernel/nortos/lib" -Wl,-i"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source/drivers/lib" -Wl,-i"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source/board/lib" -Wl,-i"C:/ti/mcu_plus_sdk_am263px_11_00_00_19/source/board/pmic/lib" -Wl,-i"C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS/lib" -Wl,--reread_libs -Wl,--diag_suppress=10063 -Wl,--diag_wrap=off -Wl,--display_error_number -Wl,--warn_sections -Wl,--gen_xml_func_hash -Wl,--xml_link_info="canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang_linkInfo.xml" -Wl,--ram_model -o "canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out" "./canfd_external_read_write.o" "./canfd_transceiver.o" "./syscfg/ti_dpl_config.o" "./syscfg/ti_drivers_config.o" "./syscfg/ti_drivers_open_close.o" "./syscfg/ti_pinmux_config.o" "./syscfg/ti_power_clock_config.o" "./syscfg/ti_board_config.o" "./syscfg/ti_board_open_close.o" "./syscfg/ti_enet_config.o" "./syscfg/ti_enet_open_close.o" "./syscfg/ti_enet_soc.o" "./syscfg/ti_enet_lwipif.o" "./syscfg/ti_sdl_config.o" "./main.o" -Wl,-l"syscfg/linker.cmd"  -Wl,-lnortos.am263px.r5f.ti-arm-clang.release.lib -Wl,-ldrivers.am263px.r5f.ti-arm-clang.nortos.release.lib -Wl,-lboard.am263px.r5f.ti-arm-clang.nortos.release.lib -Wl,-lpmic_blackbird.am263px.r5f.ti-arm-clang.nortos.release.lib -Wl,-llibc.a -Wl,-llibsysbm.a
    [110]Finished building target: "canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out"
    
    [111]C:/ti/ccs2030/ccs/utils/bin/gmake -C C:\Users\a0512372\workspace_ccstheia\canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang -f makefile_ccs_bootimage_gen OUTNAME=canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang PROFILE=Release MCU_PLUS_SDK_PATH=C:/ti/mcu_plus_sdk_am263px_11_00_00_19 CG_TOOL_ROOT=C:/ti/ccs2030/ccs/tools/compiler/ti-cgt-armllvm_4.0.3.LTS CCS_INSTALL_DIR=C:\ti\ccs2030\ccs\ CCS_IDE_MODE=desktop DEVICE=am263px
    [112] Boot multi-core ELF image: am263px:r5fss0-0:nortos:ti-arm-clang C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.mcelf ...
    [113]python C:/ti/mcu_plus_sdk_am263px_11_00_00_19/tools/boot/multicore-elf/genimage.py --core-img=0:Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out --output=C:/Users/a0512372/workspace_ccstheia/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang/Release/canfd_external_read_write_am263px-lp_r5fss0-0_nortos_ti-arm-clang.mcelf --merge-segments=true --tolerance-limit=0 --ignore-context=false --xip=0x60000000:0x68000000 --xlat=none --max-segment-size=8192
    

    Best Regards,

    Donnie Kim

  • Hi Nilabh,

    My python version was 3.13 so I reinstall the python to 3.10. and then now the stuck is solved. 

    But one thing i need is install openssl too. Probably you can hold the answer for this and I will try to install openssl first. It takes some times due to the security program block. 

    Thank you.

    Best Regards,

    Donnie

  • Hi Nilabh, 

    Now the problem is fixed. I can build it now. 

    The main problem was the python version. I think the latest python version 3.13 is not compatible with this SDK.

  • Thanks for the confirmation, Donnie. Glad to know that its working for you

  • Hi Donnie,

    I’ve started experimenting with the AM263P board just like you, and while waiting for it to arrive, I began installing all the necessary tools. Why do we need Python and OpenSSL? Can’t we just use CCS Debug to load the .hex file into RAM?

    Thanks a lot,
    Pasquale

  • Hi Pasquale,

    I'm not familiar to the background but If you want to compile the LP-AM263P SDK examples, it seems that you need to install Python and OpenSSL.

    It is not for the debug, but it is for build i think.

    Please refer to the link:https://software-dl.ti.com/mcu-plus-sdk/esd/AM263PX/11_00_00_19/exports/docs/api_guide_am263px/SDK_DOWNLOAD_PAGE.html#autotoc_md13

    Thank you.

    Best Regards,

    Donnie

  • Why do we need Python and OpenSSL? Can’t we just use CCS Debug to load the .hex file into RAM?

    Yes you can load the hex in RAM and run without installing Open SSL.

    But I would recommend installing both , as it will be needed when you want to run code from flash