Other Parts Discussed in Thread: OMAP-L138, OMAPL138
I want to use "System Reset" by ARM9 core of OMAP-L138.
I am using XDS510USB-PLUS in CCSv5.1.0.
I do "System Reset" by CCS menu or GEL script.
CCS menu is "Run - Reset -System Reset".
GEL script is "GEL_AdvancedReset("System Reset")".
When Target configuration is "Spectrum Digital XDS510USB-PLUS Emulator via JSC", "System Reset" is available,
but this target configuration is too slow speed, because it is go via the TI JSC interface.
When Target configuration is "Spectrum Digital XDS510USB Emulator", "System Reset" is not available,
but i saw that it was available in CCSv4.1.2.
"System Reset" by ARM9 core is supported by XDS510USB-PLUS?
If it is supported, what should i do to use "System Reset" by ARM9 core?
Thank you.