Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS1227, HALCOGEN
Hi,
I am trying to develop an ethernet bootloader for a different part, TMS570Ls1227, starting from a launchpad incorporating TMS570Lc4357.
I am currently stuck in trying to make the exmaple work, os far I:
- pulled latest example from git (https://git.ti.com/cgit/hercules_examples/hercules_examples/)
- tried to import in the Ethernet Bootloader exmaple under "applicatio" folder using the TMS570LC4357 HALcogen build
The first time CCS 12 didnt recognize the folders so I had to adjust manually both the Boot, lwip1.4.1 and HALcogen folder paths.
Then whenever I tired building the example i was getting an error like gmake - nothing to build; for this I created a ew project, importing the needed folders and setting the sae parameters in the project config, such as variables and incude options.
I am still stuck in building the example, which is frustrating given that it should be an exmaple so I would expect not to be so a quest to make it work; so far I have the following issues:
- fsdata.c throws me an incomplete type error

- then it tells me fsdata.c is missing reference file <dir.h>, which I honestly don't have a clue where to find

- finally lwip_check.h is missing reference file to "check.h" which I don't see anywhere

Can someone:
- point me a working example, even a simple complete project which can be built so I can start looking at how it works etc
- point me to what is actualy wrong or I am doing wrong, because I cannot understand how to make it work
- if porting then the example to a different micro should be difficult, considering that the PHY used is a DP83848 instead DP838640?
thanks