This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6416 DSK emulator Error

Hi all,

I'm using the C6416 DSK (sBox64) with CCS3.1,.

The sBox I had been using had a problem, so I asked for a new one.

However, when I try to open CC using the new sBox, the following error occurs.

"Error initializing emulator

I/O Port = 540

Board Name: DSK6416
Cpu Name: DSP_C64xxE"

when I run the 6416DSK Diagnostics, the following message comes out.

"Starting diagnostic test suite.
--> Running USB diagnostics.
Can't connect to target.

*** Plug in power and USB cable.
*** Can't run if Code Composer or Diagnostic already running.

Result> USB diagnostic fail"

However, there is no problem when I connect the old sBox.

What can be the issue?

Many Thanks,

MS