Other Parts Discussed in Thread: TMS320F28044
I have a TMS320F28044 eZdsp board and am running CCSv4 on Windows Vista. I'm trying to load a program onto my board, but the Connect Target button under the Target drop down menu is grayed out so that I cannot select it. I've been following the Build and Load Project section of C2000 Getting Started with Code Composer Studio v4,
http://processors.wiki.ti.com/index.php/C2000_Getting_Started_with_Code_Composer_Studio_v4
Under the Set up the Target Configuration Options for Device Emulation, I'm not sure which item to select under the 'Connection' drop down menu, so I have tried all of them that have my board listed. If I press the the green bug (Debug) button on the toolbar instead of attempting to do each set individually I get this message "Error initializing emulator' for every 'Connection' available. I'm not sure if this is due to me not having the option to connect to the target or not, but I'm looking for a work around this or a way to connect to the target. My goal is to have my program on my board and this sounds like the route that I need to take to get there.
Thank you,
Kevin Volz
Baylor University BSECE student