Hi,
I have a problem with the Opcode exception and have no idea how to tackle it. The abort Opcode exception is somewhat reproducible, however, if I were to insert a breakpoint in the code, the problem cannot be reproduce. Any help will be greatly appreciated.
Here is the description of the system:
Processor: c6472
BIOS: 6.31.4.27
IPC : 1.22.3.23
XDC: 3.20.8.88
XDAIS : 6.23
CCS : 4.2.4.00033
NTSR=0x1020f
ITSR=0xf
IRP=0x28cc60
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x80f694
EFR=0x2 NRP=0x80f694
Internal exception: IERR=0x8
Opcode exception
Thanks much,
Dominic