This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: project0 compiler migration fails

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: EK-TM4C1294XL

Host OS: Windows 11 Pro, Version 24H2, OS build 26100.7462

Security: Windows Defender Antivirus and Windows Firewall

Code Composer Studio Version: 20.4.0.13__1.10.0

SDK: TivaWare_C_Series-2.2.0.295

I imported project0 from the examples for the EK-TM4C1294XL using Resource Explorer.

Contents of the project that could be copied:

project0.c startup_ccs.c 

When I check the project properties:

image.png

I check the compiler dropdown

image.png

and select the only compiler available (TI Clang v4.0.4.LTS)

CCS performs migration tasks that result in the following log file: project.log 

Nothing in the forums seemed to match, so I'm trying a new post.