This is a pretty dumb question. I'm just trying to find out how to install NDK 2.2 for use with CCS5 and Sys/Bios. I've already installed CCS5 (full installation), and I've managed to migrate one simple project from CCS3.3 and build it. I now want to go on to migrate larger projects using the NDK. I know that the NDK has in the past been installed undere the DSP/BIOS. I'm not sure how it should now be installed for use with CCS5, Sys/Bios. I've downloaded the NDK zip and opened it up. I've found that the User's Guide has a section (1.2) that purports to address setup, but it seems to have no instructions whatsoever. I've been searching docs for a long time, and as embarrassing as it is, I do need help with this. I hope that someone can point me in the right direction.