Sir,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sir,
Hello Sajal,
First, what version of Code Composer Studio are you using?
Hi
I have the same problem. I use CCStudio v3.3. My windows is 32-bit. I try MATLAB 7.12 and 7.11, but the result is same.
When I type ccsboardinfo command in MATLAB, it can detect my F28335 cpu.
Thank you.
Saeid Kohan
kohansal@ieee.org
When I built the simulink model I got the following error :
Error building Real-Time Workshop target for block diagram 'dspafxr'. MATLAB error message:
Error using ==> callMakeHook.p>callMakeHook at 47
The call to ccslink_ert_make_rtw_hook, during the entry hook
generated the following error:
Error using ==> i_entryHookpoint at 52
Error while creating the link for IDE.
The build process will terminate as a result.
can someone tell me why I am getting this error please ???
I am using Matlab R2007A
CCS V3.1
c6713DSK
Plz sombody help me ???
Hello,
These are simulink error messages. I would contact Mathworks for support as they will have the most expertise.
Thanks
ki