Other Parts Discussed in Thread: LM3S6432, CCSTUDIO
I am developing a project base in Third party uip code, Initialy I compile and debug the code in IAR, the project RUN ok, I chage to CCS v5 becouse the project is bigger than 32k, however I have problems with CCS, the project compile ok without error, however, when I debug the project, I have some problems that I dont understant, after some time the project dont run ok. I think it can be a optimization problem. Do you have any recomendation to configure the project options or any other recomendation.