Hi,
I am trying to run CCS version 3.3 on a virtual machine(OS is Windows XP SP3) hosted on VMWare ESX 4.1/5.0.
All the required packages gets installed and even the drivers for the target board gets recognized automatically.
But when the CCS application is started, I get I/O error for USB enumeration.
This works fine with VMplayer though.
Has anyone tried running CCS with ESX based Virtual machines for target board 6482 DSK?
Regards,
Shashi