This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Facing issues while linking Code for TMS320C6414.

Other Parts Discussed in Thread: TMS320C6414

Hi,

A customer of mine is facing issues while linking Code for TMS320C6414.
Errors:

warning: entry point symbol _c_int00 undefined

 
>>   error: relocation overflow occurred at address 0x0000003c in section
            '.text' of input file 'D:\Sainath\DSP_Project\Debug\echoc6xxx.obj'.
             The 16-bit relocated address 0x96cc is too large to encode in the
            16-bit signed field. The value was truncated. You may need to add a
            mask to the assembly instruction or use other target specific
            assembly features if you really only need the lowest 16 bits of
            this symbol. Please see the section on Relocation in the Assembly
            User's Guide.

undefined                        first referenced
 symbol                              in file
---------                        ----------------
_c_int00                         D:\Sainath\DSP_Project\Debug\globalvar.obj
__strasg                         D:\Sainath\DSP_Project\Debug\message.obj


>>   error: symbol referencing errors - './Debug/ELU31_3_DSP.out' not built

>> Compilation failure

Build Complete,
  3 Errors, 1 Warnings, 0 Remarks.
He has  added the real time Libraries ... still the same issue .. He wants to know how to  setup for TMS320C6414 with Compiler and linker Options. His  code consists of both c and assembly language. it is non BIOS based code.. ]

 

Shimi

1-756100846