Part Number: CCSTUDIO-THEIA
Hello all,
I am using the TI SDK MMWAVE_L_SDK_06_00_05_01 with CCS version 20.4.0.13__1.10.0.
To get started, I imported the empty project and began working with it. However, I am not fully sure how to use the workspace in a collaborative development setup. For example, I need to modify configurations in FreeRTOSConfig.h and rebuild the FreeRTOS libraries to enable certain features. But it seems that FreeRTOS is provided as a precompiled library from the default SDK installation path, which prevents me from rebuilding it or keeping the dependent source files within a shared workspace.
Could you please advise if there is a recommended way to maintain a CCS‑based project collaborative setup(git repo)?
Regards,
Suba