Part Number: MSPM0G3518-Q1
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
Hello TI,
I encountered an issue while enabling Customer Security Configuration (CSC) on my ECU. After enabling CSC via BOOTCFG5 and initiating a hardware reset, I am unable to establish a connection with the ECU. The debugger indicates that the ECU is in a low power mode and refuses to establish any connection.
I have attempted the following steps to regain debugging access, without success:
- Unplugged the LaunchPad.
- Pressed and held the S1 (BSL) button.
- Plugged in the USB cable while holding S1.
- Released S1 after 2 seconds.
Additionally, I have attempted a mass erase and factory reset using both UniFlash ,BSL and CCS tools; however, no connection could be established.
Note that i configured the CSC vectortable at 0x000 and the its reset handler at 0x0004 as mentioned in the documents
Could you please provide guidance on how to resolve this issue and re-establish a debugging connection with the ECU?
This is the exact error when trying to connect using IAR

kindly find the log files from uniflash factory reset operation here