This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to download program to flash in CCSv5.1 via Stellaris ICDI

Other Parts Discussed in Thread: LMFLASHPROGRAMMER

I cann't find any command or menu item  in CCSv5.1 to download program to flash, so I have to start a debug session to run my app. Troublesome!

Is there any soluthion? Eclipse plugin?

My platform is:  LM4F232 Evaluation Board (Cortex-M4), Stellaris ICDI

Thanks.

  • Hi Kim,

    Unfortunately for Stellaris there is no built in flash programmer in CCS.   There is a free flash programmer for the Stellaris micros available here however for you to use:

    http://www.ti.com/tool/lmflashprogrammer

    Best Regards,
    Lisa

  • Kim,

    Just a small clarification; what Lisa means is that there is no standalone flash programmer in CCS, as the built-in CCS debugger is able to perform flash programming in Stellaris devices.

    Somehow I was a bit confused by the term built-in flash programmer... :)

    Cheers,

    Rafael

     

  • Hi Lisa,

    Thanks for the fast response.

    I started using the standalone tool LM Flash Programmer as the begining, although it is powerful, but not so convenient.

    Other IDE, such as Keil, support a download button on the toolbar, when I edit my code, click the button, it can download, reset mcu and run automaticly, just one click .

    Thanks

  • It is unclear to me what this means. I am assuming that there is an integrated flash memory programmer in the CCS v5. Does this occur through the debugger via the Load option? Or is there another option I don't see.