Other Parts Discussed in Thread: CCSTUDIO
I'm running CCS5 5.1.0.09000 and whenever the target is disconnected and the CPU reset button is hit, the application crashes and needs to be restarted from scratch. Is this normal operation?
Also, is there a way to have the debug buttons (run,step,step into, etc) available on the tool bar without the need for the debug window to be open? I don't need to know the status of my debug when I'm stepping, so having that window open just wastes space on the desktop.
Thanks.