Hi,
Need help for advise on the compatibility issue of the CCS v4.2.3 with the Windows 7 64bit.
Currently using the EKS-LM3S9B92. Followed the Userguide closely and everything behaved as the guide until the instruction of click Debug Active Project. Nothing happened, i.e no connection was established to the board. Subsequently CCS hang at start-up every time at the point where it is trying to load the workbench.
Later managed to have the board connection, which took more than 7 minutes.
However, my system encounter problems like bluescreen whereby I believe it is some conflict but I have only the mouse and keyboard connected.
Tried to install the same into the Windows XP, and everything seems to run smoothly.
Kindly advise on how to resolve the issue. Do advise if there is any additional information required to help me to solve the problem. Thanks.
regards,
RVG