Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG, AM2631, AM263P4
I am new to Texas Instruments microcontrollers and currently starting development with the Texas Instruments AM2634 MCU using the MCU+ SDK.
While setting up the development environment, I noticed that there are different versions of Code Composer Studio, such as CCS 12.8 (Eclipse-based) and the newer CCS 20.4.1 (Theia-based). The newer CCS v20 is based on a different IDE framework (Theia) and has a different workflow compared to the older Eclipse-based CCS versions.
Since I am just beginning with TI microcontrollers and have not used either version before, I would like some guidance from TI experts.
My questions are:
For a beginner starting with AM2634 and MCU plus SDK, which Code Composer Studio version is recommended to use?
Is it still acceptable to start development using CCS 12.8, or is it better to directly use CCS 20.x?
Are there any compatibility issues with MCU plus SDK, SysConfig, or drivers if older CCS versions are used?
For applications involving Ethernet, SPI, and UART, does the choice of CCS version affect development or debugging?
Any recommendation on which CCS version is better to start with for new users would be very helpful.
While exploring the Code Composer Studio Resource Explorer and the Texas Instruments Training Academy, I noticed that each MCU plus SDK release seems to require a specific version of CCS, compiler, and SysConfig.
From the documentation, it appears that every SDK is validated with particular tool versions (CCS, compiler, SysConfig).
I would like to confirm if my understanding is correct.
If so, I have a few questions:
Is it recommended to use the exact CCS, compiler, and SysConfig versions specified for a given SDK?
If I start development using an older SDK with the corresponding older CCS version, is that still a good approach for learning and development?
Or is it better to start directly with the latest CCS and latest SDK versions for new projects?
I would appreciate guidance on which approach is generally preferred when starting development with Texas Instruments AM2634.