This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5 nested headers

Other Parts Discussed in Thread: MSP430G2211

I recently upgraded to CCS 5 and noticed some of my old CCS 4 projects that employ nested header files do not work anymore.  It appears that the mspx2xx1 header file which is defined in A.h  is not showing up when I include A.h in a project.  Does anyone know how to fix this?  The code used in the project is:

Code: A.h

#ifndef MCU_H_
#define MCU_H_
    #include <msp430g2211.h>  //Processor Selection (Replace with processor you are using)
    #define CLK_Speed 0x3   //Processor Speed in Megahertz
    
    #define _PWM_Port_1
#endif /*MCU_H_*/

Code: Project

#include "A.h"

#include"PULSE_Power.h"


void main(void){
    WDTCTL =WDTPW + WDTHOLD;    //Disable Watchdog
    
    BCSCTL1 = CALBC1_1MHZ;
    DCOCTL = CALDCO_1MHZ; // D

    PULSE();

}

This project returns error saying that the symbols (WDTCTL, BSCTL1, etc.) are undefinedThe pulse function however is defined.