This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-570LC43: Issue flashing TMS570LC43 LaunchPad using UniFlash with .bin file

Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: UNIFLASH

Device / Tools:

  • MCU: TMS570LC43xx (Hercules)
  • Board: TMS570LC43x LaunchPad
  • CCS Version: CCS 12.8.1 / TI v20.2.7.LTS compiler
  • UniFlash Version: (9.4.1 )
  • Debug Probe: XDS110

 

I am able to successfully flash and run my application using Code Composer Studio (CCS) using Debug and Flash mode.and able to  the generated .out and .Bin  file.
However, when generating a .bin file using through UniFlash, the flashing completes successfully but:respective Device is not working properly.    

image.png

fa102f48-3a56-4e79-a268-3f86662952fb.png