This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2332: Assembly Program on IAR and CCS not compitible.

Part Number: MSP430G2332

Dear friends :

My problem is as followings:

Assembly program by IAR is work correctly. But, almost same Assembly program by CCS is not work as by IAR.

The IAR assembly program and CCS project fold are attached.

main.asm AS-V9-128-flash-Fewrite-Fix-2026b-s43.txt 

I need help !

Thanks to all !

Marshall Wu 2026/03/19

  • Hello Marshall,

    Did you use assembly as below steps? And in fact, we have one guide, maybe you can try to check whether you can find what you want in the guide

    MSP430 Assembly Language Tools v16.9.0.LTS (Rev. M)

    Best Regards,

    Janz Bai

  • Dear Janz Bai:

      Thanks a lot for your prompt response.

      CCS assemble program make to generate *.out is ok!

      The problem is the hardware interrupt response too slow, so certain function are not work as program make by IAR.

       Could you tell me how to solve such kind of problem ?

       how to speed-up the interrupt response time ?

       Best regards;

       Marshll Wu 2026/03019

  • CCS Main.asm and IAR ***.S43 are attached as followings.

    5078.main.asm

  • IAR ***.S43 can not be accept by system, So ***.S43 change to ***-s43.txt

    #include "msp430g2332.h"                     ; #define controlled include file
    //******************************************************************************
    //  AddrSdModule
    //  address: A0~A6 = p1.7,p2.1,p2.2,p2.3,p2.4,p2.5,p2.6 
    //  R-LED=p1.4, G-LED=p1.6, ACK=PB1=p1.1
    //  OP-pwr=p1.3, Ain=P1.0  AD-10 ch1, PIR-p1.2 output
    //  clk=p1.5, data=p2.0 ack=p1.1
    //  Built with IAR Embedded Workbench Version: 6.40
    //******************************************************************************
    // the last 3 sum >160/170 alarm otherwise normal 2013/09/25
    // >=53 alarm else normal 2013/09/14
    // >=55 alarm else normal 2013/09/16
    // SdDetecor.s43 copied from TdDetector.s43 2013/06/25
    //TdDetector copied from SmartaNew1221.s43  2013/06/24
    //Program SmartaNew1221.s43 COPIED FROM SmartaNew1102.s43 FOR max bitcnt=16
    //  variable declare segment
    // AddrSdDetector-V2 copied from AddrSdDetector-V1 2014/02/11
    // AddrSdDetector-V3 copied from AddrSdDetector-V2 2014/02/19
    // greater  than 0x8d then count 3 up, if less than  0x8d then decrese 1 
    // PB6=p1.4 no PB7=P1.6 Green LED 2014/04/17
    // use enhance gain 12.5% for stable after 1st alarm level. 2014/04/21
    // use sum-up the last 5 samples to determinate the alarm level 650 ALRMW
    // add fault function if OP output less than #40 means skoke charmber dirty
    // update from AddrSdDetector-V61.s43  2014/05/14 
    // update from V7 for ignor #128 cmp, and twice to alarm
    // update from V8 for 256 node
    //2014/07/18 tested OK! by Marshall
    //2014/11/10 AddrSdDetector-V8-256a.s43 enhance gain 1/4=25%
    //MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2014/12/03
    //2015/01/06 switch to -VT for debug !
    //2015/05/11 alarm = 650 single =130 max.alarmcnt 6 
    //2015/10/02 modify p1.6 for testing command
    //2015/11/27 use base value to adjust the measure result.
    //standard base value=69; Adj=69*64/Base-n then value * Adj / 64
    // copy from AddrSdModule-Type2a-V9-Fe-20160129-ADJ 2024/12/03
    // MOV     #120,&FireVal     ;modify this vale for sensibility of smoke 2025/02/17
    //copy from AddrSd-128-14Type2a-V9-Fe-20241203-ADJ -RLY 2025/11/24
    //remove fault detector charmber dirty 
    //copy from AddrSd-128-14Type2a-V9-Fe-20241203-20251125-ADJ -RLY - 188
    // add ActFlag to inhibit ADJ function 2025/11/26
    //2025/11/29 updated, not test yet !
    //
    
    DOCNT   EQU   0200h
    HICNT   EQU   0201h
    LASTHI  EQU   0202h
    ADDR    EQU   0203h
    CFLAG   EQU   0204h
    RCVHI   EQU   0205h
    RCVLO   EQU   0206h
    STK1    EQU   0207h
    CNT4    EQU   0208h 
    //CNT5    EQU   0209h
    SYSAD1  EQU   020Ah
    SYSAD2  EQU   020Bh
    SYSAD3  EQU   020Ch
    DO1     EQU   020Dh
    DO2     EQU   020Eh
    DO3     EQU   020Fh
    DO4     EQU   0210h
    DO5     EQU   0211h
    CNT1    EQU   0212h
    CNT2    EQU   0213h
    DFLAG   EQU   0214h
    BITCNT  EQU   0215h
    CADDR   EQU   0216h
    COUT    EQU   0217h
    CIN     EQU   0218h
    XMTIN   EQU   0219h 
    WORK    EQU   021Ah
    LPCNT   EQU   021Bh
    RLYON   EQU   021Ch
    FRMCNT  EQU   021Dh
    FireVal EQU   021Eh    ;alarm value-L
    CST2    EQU   021Fh    ;alarm value-H
    ADDRL   EQU   0220h    ;not use
    FCNT1   EQU   0221h    ;pooling flash count
    DADDR   EQU   0222h
    EADDR   EQU   0223h
    BKRLY   EQU   0224h
    MANFLG  EQU   0225h
    WARM1   EQU   0226h
    WARM2   EQU   0227h
    WARM3   EQU   0228h
    WARM4   EQU   0229h
    PARITY  EQU   022Ah
    WDCNT   EQU   022Bh
    WKR2    EQU   022Ch
    CCS     EQU   022Dh
    FSLEEP  EQU   022Eh   ;SLEEP FLAG
    FLASH   EQU   022Fh   ;FLASH ONCE FOR 10 TIMES ADDRESSED
    FAULT   EQU   0230h   ;FAULT STATUS FLASH COUNT 0=INITIAL
    TMCNT   EQU   0231h   ;TIMER CNT  6/SEC AT 3MHz **************
    PORT1IN EQU   0232h   ;PORT1 INPUT
    PORT2IN EQU   0233h   ;PORT2 INPUT
    CNT_SET EQU   0234h   ;RELAY SET COUNTER 2  5~10 ms
    CNT_RST EQU   0235h   ;RELAY RESET COUNTER 2  5~10 ms
    RLY_FLAG EQU  0236h   ;RELAY SETTING FLAG
    RLY_STS EQU   0237h   ;RELAY STATUS 
    ADRCNT  EQU   0238h   ; GET ADDRESS COUNTER
    RLYDOX  EQU   0239h   ;relay check templary work byte
    RLYCNT  EQU   023Ah   ;use for gain and flash led flags.0x12h
    SENCNT  EQU   023Bh   ;SMOKE SENSE TIMER, INITIAL 4S, 2ND 1S, 3RD ALARM
    SENTM   EQU   023Ch   ;smoke sense timer, 10 sec/4 sec/1sec
    SENFLAG EQU   023Dh   ;sense flag trig smoke sense
    TSTCNT  EQU   023Eh   ;Smoke test cnt
    ALMCNT  EQU   023Fh   ;alarm count
    ;
    SMKD1   EQU   0240h   ;DARK SENSE  
    SMKD2   EQU   0242h   ;DARK SENSE  
    SMKD3   EQU   0244h   ;DARK SENSE  
    SMKD4   EQU   0246h   ;DARK SENSE 
    SMKL1   EQU   0248h   ;LIGHT SENSE  
    SMKL2   EQU   024Ah   ;LIGHT SENSE  
    SMKL3   EQU   024Ch   ;LIGHT SENSE  
    SMKL4   EQU   024Eh   ;LIGHT SENSE
    SMKR1   EQU   0250h   ;avg. of dark sense  
    SMKR2   EQU   0252h   ;acg. of light sense  
    SMKR3   EQU   0254h   ;diff. of light - dark  
    INDEX   EQU   0256h   ;LIGHT SENSE
    MINW    EQU   0258h   ;MIN value
    MINRSTW EQU   025Ah   ;MIN reset value
    WORKW   EQU   025Ch   ;
    ALRMW   EQU   025Eh   ;Alarm value
    ADJ     EQU   0260h   ;adj vaule
    STDBASE EQU   0262h   ;69 * 64
    WORKA   EQU   0264h    ;
    WORKB   EQU   0266h 
    WORKC   EQU   0268h
    WORKD   EQU   026Ah
    WORKE   EQU   026Ch
    LOWEST  EQU   026Eh    ;LOWEST BASE VALUE
    LOWEST1 EQU   026Fh
    BIGCNT  EQU   0270h    ;GREATER COUNTER, ADD 1 IF TEST VALUE > LOWEST
    DOCNT16 EQU   0272h
    SMKRAW  EQU   0274h     ;raw data before adiusted.
    FEWRT   EQU   0276h     ;LOWEST SETTED FLAG
    ADCFLAG EQU   0278h     ;ADC10 Flag
    FaulVal EQU   027ah     ;fault value = LOWEST / 2;
    ActFlag EQU   027ch     ;alarm active flag set by alarm, reset as alarm clear 2025/11/26 
    NorFlag EQU   027dh     ;normal running 2025/11/27
    LowCnt  EQU   027eh     ;lower than LOWEST counter
    LOGTBL  EQU   0280h   ;result buffer
    
    
    ;
    F_IN    EQU   0x01
    F_WD    EQU   0x02
    F_MAT   EQU   0x04
    F_OUT   EQU   0x08
    F_BIT   EQU   0x10
    F_POST  EQU   0x20
    F_PAS   EQU   0x40
    F_SYS   EQU   0x80
    F_RLY   EQU   0x80
    F_SET   EQU   0x01
    F_RST   EQU   0x10
    ;
    
    
            ORG     0F000h
           
    init:   MOV     #0300h, SP        ; set up stack
            MOV.B   #060h,&DCOCTL
            MOV.B   #089h,&BCSCTL1    ;89 = 3MHz
            CLR.B   &BCSCTL2
            CLR.B   &BCSCTL3
            BIC.B   #OFIE,&IE1
            BIC     #LPM4,SR
            MOV     #100,&ADRCNT
            MOV.B   #150,&TMCNT         ;INITIAL TIMER COUNTER **************
            MOV.B   #100,&WDCNT
            MOV     #15000,&TACCR0
            MOV     #0212h,&TACTL     ;INITIAL TIMER_A  1/1, SMCLK, UP MODE
            MOV.B   #10,&SENTM
            MOV.B   &SENTM,&SENCNT
            CLR.B   &SENFLAG
    ;         MOV.B   #6,&TMCNT         ;INITIAL TIMER COUNTER **************
    ;         MOV     #02E2h,&TACTL     ;INITIAL TIMER_A      **************
            CLR.B   &CNT_SET
            CLR.B   &CNT_RST
            CLR.B   &RLY_FLAG
            CLR.B   &RLY_STS
            CLR.B   &DO1
            CLR.B   &DO2
            CLR.B   &DO3
            CLR.B   &RLYON
            CLR.B   &RLYCNT
            CLR.B   &ActFlag          ;2025/11/26
            CLR.B   &NorFlag          ;2025/11/27
            CLR     &LowCnt
            MOV     #LOGTBL,R5 
            CLR     0(R5) 
            CLR     2(R5)
            CLR     4(R5)
            CLR     6(R5)
            CLR     8(R5)
            CLR     10(R5)
            CLR     12(R5)
            mov     #64,&ADJ
    //        MOV     #180,&FireVal     ;modify this vale for sensibility of smoke 2025/02/17  (120->150 2025/11/24)
            MOV     #270,&FireVal     ;modify this vale for sensibility of smoke 2026/03/10  (180->270 2026/03/10) 180*1.5
    
    //SetupWDT    mov.w   #WDTPW+WDT_ADLY_1000,&WDTCTL  ; WDT 1s*4 interval timer
    //SetupBC     bis.b   #DIVA_2,&BCSCTL1        ; ACLK/4
    //            bis.b   #WDTIE,&IE1             ; Enable WDT interrupt
          // PORT 1 CONFIGRATION
    //        MOV.B   #0x01,&ADC10AE0      ;enable A0
    //        MOV.B   #0eeh,&P1OUT       ;P1 PULL-UP RESISTOR=1110-1110
            MOV.B   #0eeh,&P1OUT       ;P1 PULL-UP RESISTOR=1110-1110 2024/12/03 P1.6 low active
    //        MOV.B   #01eh,&P1DIR       ;P1 0001-1110 P1.5 CLK, p1.7 add8,p1.0 ad0, p1.6=test in
            MOV.B   #05eh,&P1DIR       ;P1 0101-1110 P1.5 CLK, p1.7 add8,p1.0 ad0, p1.6=relay output
            MOV.B   #000h,&P1SEL       ;P1.0, p1.3 for ad0, op-pwr, ALL othrs DIGITAL I/O
            MOV.B   #000h,&P1SEL2
    //        MOV.B   #0A6h,&P1REN       ;1010-0110 ENABLE PULL-UP RESISTORS
    //        MOV.B   #0E0h,&P1REN       ;1110-0100 ENABLE PULL-UP RESISTORS p1.1 no pull-up/down
            MOV.B   #0A0h,&P1REN       ;1010-0100 ENABLE PULL-UP RESISTORS p1.1 no pull-up/down
            MOV.B   #020h,&P1IES       ;SELECT P1.5 HI->LO EDGE INTERRUPT
            CLR.B   &P1IFG             ;CLEAR INT FLAGS
            MOV.B   #020h,&P1IE        ;ENABLE P1.5 INT clk
          // PORT 2 CONFIGURATION 
            MOV.B   #0FFh,&P2OUT       ;P2.0,1,4,5,6,7 PULL-UP HIGH P2.6 ACTIVE LOW
            MOV.B   #000h,&P2DIR       ;P2.0=data, p2.1p2.7 +p1.7  address
            CLR.B   &P2SEL             ;PORT 2 ALL DIGITAL I/O
            MOV.B   #0FFh,&P2REN       ;EN UP/DOWN R all
            MOV.B   #001h,&P2IES       ;SELECT P2.0 HI->LO EDGE INTERRUPT
            CLR.B   &P2IFG             ;CLEAR INT FLAGS
            MOV.B   #001h,&P2IE        ;ENABLE P2.4 INT FOR DATA
    //ADC-10 CONFIGULATION
            BIC.W   #ENC,&ADC10CTL0 
            MOV.W   #0x0018,&ADC10CTL0
            MOV.W   #0x0000,&ADC10CTL1   ;repeat single channel
            MOV.B   #0x01,&ADC10AE0      ;enable A0
            MOV.B   #0x00,&ADC10DTC0
            MOV.B   #0x00,&ADC10DTC1     ;4 per block 
            MOV.W   #0x0240,&ADC10SA     ;start address 
            BIS.B   #0x08,&P1OUT         ;power off OP  p1.3 active low
    //END OF ADC-10 CONFIGULATION
       // TEST SEG
    //         MOV     #WDTPW+WDTCNTCL,&WDTCTL  ; watchdog timer
             MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2014/12/03
    //11/28         BIS.B   #WDTIE,&IE1
     
    //         MOV     #WDTPW+WDTHOLD,&WDTCTL
    //         BIC.B   #WDTIE,&IE1
            BIS     #GIE,SR
            MOV     #100,R14
      // END OF TEST SEG    
          // CHECK TO SEE WHETHER POWER-ON
            MOV.W   #0200h,R5 
            MOV.W   #0128,R6
            MOV.B   #010,&FLASH
    //        CMP.B   #055h,&WARM1
    //        JEQ     W2
            JMP     LSOP
    W2:     CMP.B   #0AAh,&WARM2
            JEQ     W3
            JMP     LSOP
    W3:     CMP.B   #055h,&WARM3
            JEQ     W4
            JMP     LSOP
    W4:     CMP.B   #0AAh,&WARM4
            JEQ     GETAD
    LSOP:   CLR.B   0(R5)      ;CLEAR VARIABLE
            INC     R5
            DEC     R6
            JNZ     LSOP
            MOV.B   #055h,&WARM1
            MOV.B   #0AAh,&WARM2
            MOV.B   #055h,&WARM3
            MOV.B   #0AAh,&WARM4
            MOV.B   #010,&FLASH
            CLR.B   &TSTCNT          ;test cnt 5~=5 sec
            CLR.B   &ALMCNT          ;cnt to 3 alarm
            MOV.B   #150,&TMCNT         ;INITIAL TIMER COUNTER **************
            MOV.W   #200,&CNT4
            MOV.W   #500,&LOWEST
    //        mov.w   #4416,&STDBASE   ;69 * 64 = 4416
    //        mov.w   #4992,&STDBASE   ;78 * 64 = 4992 2016/01/05
            mov.w   #7488,&STDBASE   ;117 * 64 = 7488 2026/03/10 (78*1.5)
            clr.w   &BIGCNT
            MOV.B   #100,&WDCNT
            MOV.B   #5,&FCNT1
    ; check Lowest parameter       
            mov.w   #01040h,R5
            cmp   #0xFFFF,0(R5)
            jne     Irestr
            jmp     Inxt
    Irestr: mov.b   0(R5),&LOWEST
            mov.b   1(R5),&LOWEST1
            mov.b   #0x77,&FEWRT
            mov.b   #77,&NorFlag      ;2025/11/27
            clr.w   &BIGCNT
            mov.w   &LOWEST,&FaulVal
            rra.w   &FaulVal
            MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2015/11/28
            call    #DIVID2             
            call    #MULTADJ
    ;
    Inxt:   clr     &INDEX
            mov     #LOGTBL,R10      
    ;*********************************       
    ;        mov     #780,&ALRMW      ;set alarm level value here !!! old=600
    ;        mov     #600,&ALRMW      ;set alarm level value here !!! old=600
    ;        mov     #650,&ALRMW      ;set alarm level value here !!! 2015/05/11
    ;       mov     #575,&ALRMW      ;set alarm level value here !!! 2015/11/29 use adj
    ;        mov     #600,&ALRMW      ;set alarm level value here !!! 2015/11/29 use adj
    ;        mov     #675,&ALRMW      ;set alarm level value here !!! 2025/11/25 use adj for FirVal=135
    ;        mov     #900,&ALRMW      ;set alarm level value here !!! 2025/11/25 use adj for FireVal=180
            mov     #1350,&ALRMW      ;set alarm level value here !!! 2025/11/25 use adj for FireVal=270
    ;
    GETAD:  MOV.B   &P1IN,PORT1IN    ;GET ADDRESS
            MOV.B   &P2IN,PORT2IN    ;GET ADDRESS
            INV.B   &PORT1IN
            INV.B   &PORT2IN
            CLR.B   &EADDR         ;P1.1-P1.7 DEVICE ADDRESS
            BIT.B   #80h,&PORT1IN     ;P1.7= ADDR.0
            JZ      GAD1
            BIS.B   #01h,&EADDR
    GAD1:   BIT.B   #02h,&PORT2IN     ;P2.1=ADDR.1
            JZ      GAD2
            BIS.B   #02h,&EADDR
    GAD2:   BIT.B   #04h,&PORT2IN     ;P2.2=ADDR.2
            JZ      GAD3
            BIS.B   #04h,&EADDR
    GAD3:   BIT.B   #08h,&PORT2IN     ;P2.3=ADDR.3
            JZ      GAD4
            BIS.B   #08h,&EADDR
    GAD4:   BIT.B   #10h,&PORT2IN     ;P2.4=ADDR.4
            JZ      GAD5
            BIS.B   #10h,&EADDR
    GAD5:   BIT.B   #20h,&PORT2IN     ;P2.5=ADDR.5
            JZ      GAD6
            BIS.B   #20h,&EADDR
    GAD6:   BIT.B   #40h,&PORT2IN     ;P2.6=ADDR.6
            JZ      GAD7
            BIS.B   #40h,&EADDR
    GAD7:   BIT.B   #80h,&PORT2IN     ;P2.7=ADDR.7
            JZ      GAD8
            BIS.B   #80h,&EADDR 
    GAD8:   AND.B   #07Fh,&EADDR; 
     
            //JNZ     AD0
     
    FNRM:   //BIC.B   #40h,&P1OUT     ;LIT OFF GREEN LED p1.6GREEN P1.4RED
    
    AD0:    CLR.B   &PARITY
            BIT.B   #01h,&EADDR
            JZ      AD1
            XOR.B   #01h,&PARITY
    AD1:    BIT.B   #02h,&EADDR
            JZ      AD2
            XOR.B   #01h,&PARITY
    AD2:    BIT.B   #04h,&EADDR
            JZ      AD3
            XOR.B   #01h,&PARITY
    AD3:    BIT.B   #08h,&EADDR
            JZ      AD4
            XOR.B   #01h,&PARITY
    AD4:    BIT.B   #10h,&EADDR
            JZ      AD5
            XOR.B   #01h,&PARITY
    AD5:    BIT.B   #20h,&EADDR
            JZ      AD6
            XOR.B   #01h,&PARITY
    AD6:    BIT.B   #40h,&EADDR
            JZ      AD7
            XOR.B   #01h,&PARITY
    AD7:    BIT.B   #01h,&PARITY
            JZ      W5
    AD8:    BIS.B   #080h,&EADDR       ;PUT ON PARITY BIT MAKE EVEN PARITY
    /*        
    AD7:    BIT.B   #80h,&EADDR
    JZ      AD8
            XOR.B   #01h,&PARITY
    AD8:    CLR.B   ADDRL
            RRC.B   EADDR
            RRC.B   ADDRL
            AND.B   #7Fh,&EADDR
            BIT.B   #01h,&PARITY
            JZ      W5
    AD9:    BIS.B   #080h,&EADDR       ;PUT ON PARITY BIT MAKE EVEN PARITY
    */
    W5:     MOV.B   &EADDR,&ADDR       ;MOV EADDR TO ADDR
            TST.B   &ADDR
    //        JZ      LOOP
     
            
            EVEN
    LAOP:   NOP
            BIT.B   #F_MAT,&CFLAG
            jnz     LOOP
            CMP.B    #02,&TSTCNT
            jl      LOOP
            clr.b   &TSTCNT
            bic.w   #ENC,&ADC10CTL0 
    //        nop
            //test AD10
    //StopWDT     mov.w   #WDTPW+WDTHOLD,&WDTCTL  ; Stop WDT
    SetupADC10  mov.w   #CONSEQ_2+INCH_0,&ADC10CTL1 ; Repeat single channel, A0
                mov.w   #ADC10SHT_2+MSC+ADC10ON+ADC10IE,&ADC10CTL0 ;
                bis.b   #01h,&ADC10AE0          ; P1.0 ADC option select
                mov.b   #004h,&ADC10DTC1        ; 32 conversions
    //
    Mainloop    bis.b   #04h,&P1OUT               ;IR LED off
    // 
                MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer  ;2014/12/03
                bic.w   #ENC,&ADC10CTL0         ;
    busy_test   bit     #BUSY,&ADC10CTL1        ; ADC10 core inactive?
                jnz     busy_test               ;
                mov.w   #0240h,&ADC10SA         ; dark Data buffer start
    //            bis.b   #010h,&P1OUT            ; P1.4 = 1
                bis.w   #ENC+ADC10SC,&ADC10CTL0 ; Sampling and conversion start
                mov.b   #77,&ADCFLAG
    dlop:       nop
                TST.B   &ADCFLAG
                jnz     dlop
    //            bis.w   #CPUOFF+GIE,SR          ; LPM0, ADC10_ISR will force exit
     
                bic.w   #ENC,&ADC10CTL0         ;
                bic.b   #04h,&P1OUT             ;IR LED ON
                mov     #500,R7
    //            MOV     #WDTPW+WDTCNTCL,&WDTCTL  ;WAKE WATCHDOG
                MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2014/12/03
    delaylp     dec     R7
                jnz     delaylp
    //            MOV     #WDTPW+WDTCNTCL,&WDTCTL  ;WAKE WATCHDOG
                MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2014/12/03
                EVEN
    busy_t      bit     #BUSY,&ADC10CTL1        ; ADC10 core inactive?
                jnz     busy_t                  ;
                mov.w   #0248h,&ADC10SA         ; Light Data buffer start
                bis.w   #ENC+ADC10SC,&ADC10CTL0 ; Sampling and conversion start
                mov.b   #77,&ADCFLAG
    slop:       nop
                TST.B   &ADCFLAG
                jnz     slop
    //            bis.w   #CPUOFF+GIE,SR          ; LPM0, ADC10_ISR will force exit
                bis.b   #04h,&P1OUT            ; P1.3 = 0 IR LED OFF
                bis.b   #08h,&P1OUT            ;OP Power off
                mov.w   &SMKD1,R5
                add.w   &SMKD2,R5
                add.w   &SMKD3,R5
                add.w   &SMKD4,R5
                rra.w   R5                  ;divide by 2
                rra.w   R5                  ;divide by 4
                mov.w   R5,&SMKR1
                mov.w   &SMKL1,R5
                add.w   &SMKL2,R5
                add.w   &SMKL3,R5
                add.w   &SMKL4,R5
                rra.w   R5
                rra.w   R5
                mov.w   R5,&SMKR2
                mov.w   R5,&SMKR3
                sub.w   &SMKR1,&SMKR3
                mov.w   &SMKR3,&SMKRAW 
                tst.b   &NorFlag        ;2025/11/29
                jz      nortst         ;not initialized
                cmp.w   &LOWEST,&SMKR3 
                jl      adjnxt
                JEQ     adjnx2
                clr     &LowCnt
                inc.w   &BIGCNT
                cmp.w   #30000,&BIGCNT   ;2015/11/29 300 => 30000 sec.
                jl      adjnx2
                clr.w   &BIGCNT
    //            inc.w   &LOWEST
                jmp     adjnx1
    J2init: NOP
            JMP     init              
    ;
    adjnxt:     inc     &LowCnt
                cmp     #1000,&LowCnt
                jl      adjnx0
    //            sub     #1,&LOWEST
                clr     &LowCnt
    /*
                cmp.b   #0x77,&FEWRT
                jeq      adjnx0
                mov.w     #WDTPW+WDTHOLD,&WDTCTL  ;stop watch dog
                call    #WrtLow
                mov.b   #0x77,&FEWRT
    */            
    adjnx0:     clr.w   &BIGCNT 
    adjnx1:      MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2015/11/28
                 call    #DIVID2             
    adjnx2:      call    #MULTADJ
    //            cmp     #40,&SMKRAW      ;if less than 40 means smoke charmber dirty
    //            cmp     &FaulVal,&SMKRAW   ;if less than 1/2 original means smoke charmber dirty
    //            jge     nornxtb
    //            bic.b   #01h,&XMTIN    ; set fault flag  20250207 bis->bic force to no charmber dirty
    //            jmp     nornxt         
    
    //nornxtb     bic.b   #01h,&XMTIN    ; clear fault flag            
    nornxt      bit.b   #10h,&RLYCNT      ;test for gain change
                jz      nortst           ;if not alarm goto nortst
    //            mov.b   #03,&TSTCNT    ;next second test again
    //            mov.w   R5,&SMKR3
                mov.w   &SMKR3,R5
                rra.w   R5
                rra.w   R5        ;divid 4 =25%
                rra.w   R5     ;divid 8 =12.5 %  2015/11/29 setted
                add.w   R5,&SMKR3       ;plus 12.5%
    nortst      mov     &SMKR3,0(R10) 
                incd    R10
                inc     INDEX
                cmp     #6,&INDEX
                jne     LP_NORB
    //            mov.b   #77,&NorFlag
                mov      #LOGTBL,R6
                mov      10(R6),12(R6)
                mov      #5,R7
    mvlp        mov      2(R6),0(R6) 
                incd      R6
                dec      R7
                jnz      mvlp
                dec      &INDEX
                cmp.b   #0x77,&FEWRT 
                jeq      pronxt
                mov.w     #WDTPW+WDTHOLD,&WDTCTL  ;stop watch dog
                call    #WrtLow
                mov.b   #0x77,&FEWRT
                mov.b   #77,&NorFlag
                mov.w   &LOWEST,&FaulVal
                rra.w   &FaulVal
    pronxt      mov      #LOGTBL+10,R10    ;reset table index
    
                mov      #LOGTBL+10,R9 
                mov      @R9,&WORKW        ;the last one
                add      -2(R9),&WORKW     ;new
                add      -4(R9),&WORKW
                add      -6(R9),&WORKW     ;old
                add      -8(R9),&WORKW     ;5 samples sum
                jc       nortst0  
                cmp      &ALRMW,&WORKW       ;test sum 5 samples
                jl       nortst2         ;ignor #128 
    nortst0     add.b    #1,&ALMCNT
                jmp      nortst3          ;rise rate high       
    ;nortst2     cmp      #180,&SMKR3      ;0x80  old=130 2014/11/10  
    ;nortst2     cmp      #130,&SMKR3      ;0x80  old=130 2014/12/03
    ;nortst2     cmp      #115,&SMKR3      ;0x80  old=130 2015/11/29 use adj
    ;  &ALRMW = #120 * 5 = 600   &FireVal
    ;nortst2     cmp      #120,&SMKR3      ;0x80  old=130 2016/01/05 use adj newchamber
    nortst2     cmp      #270,&SMKR3      ;0x80  old=130 2025/11/25 use adj newchamber
                jl      LP_NORB          ; 
    //            mov.b   #03,&TSTCNT    ;next second test again
    //            add.b   #1,&ALMCNT
                add.b   #2,&ALMCNT       ;2014/12/04
    nortst3     bis.b   #10h,&RLYCNT     ;for gain + 12.5% 
                add.b   #1,&ALMCNT
                bic.b   #08h,&P1OUT             ;op power on low active 
                mov.b   #1,&TSTCNT              ;shorten sampling time
                cmp.b   #6,&ALMCNT     //count 3 to alarm old=4
                jl      LOOP
                mov.b     #99,&ActFlag   //set for inhibit ADJ
                bis.b   #02h,&XMTIN    //set fire flag
                bis.b   #02h,&RLYCNT
                bis.b   #10h,P1OUT     //lit red led
                CLR.B   &FLASH
    //            inc.b   &ALMCNT
                cmp.b   #12,&ALMCNT     //6->8 2025/11/26
                jl      LOOP
                mov.b   #12,&ALMCNT     //6->8 2025/11/26
                jmp     LOOP
       //end of test AD10
    //J2init: NOP
    //        JMP     init  
    LP_NORB: 
    //         bit.b   #040h,&P1IN         //test test reed switch 
    //         jnz      LP_NORBB
    //         add.b   #6,&ALMCNT         //if zero=contact emulate alarm
    //         jmp     nortst3
    LP_NORBB: tst.b   &ALMCNT
             jz      LP_OK
             dec.b   &ALMCNT
             jnz     LOOP   
    LP_OK:   EVEN
             clr.b   &ActFlag     //clear ActFlag
             bic.b   #02h,&XMTIN     //reset fire flag
             bic.b   #10h,P1OUT      // off red led
             bic.b   #12h,&RLYCNT    ;
    //         clr.b    &TSTCNT
    //         mov.b   #10,&SENTM
    //         mov.b   #10,&SENCNT
          
             
            EVEN
            
    LOOP:   CMP.B   #17,&BITCNT    ;#18
            JL      LP_NORM
            CLR.B   &BITCNT
            EVEN
    LP_NORM: BIT.B   #F_IN,&DFLAG
            JNZ     LPIN
            DEC.B   &WDCNT
            JNZ     LPWDT
    //        MOV     #WDTPW+WDTCNTCL,&WDTCTL  ;WAKE WATCHDOG
            MOV     #WDTPW+WDTCNTCL+WDTSSEL,&WDTCTL  ; watchdog timer 2014/12/03
            MOV.B   #20,&WDCNT       ;old 100 2014/11/10
            JMP     GETAD
            EVEN
    LPWDT: // TST.B   &ADDRL
           // JNZ     LPNN
            TST.B   &ADDR      ;IF ADDR == 0
            JZ      DIOS      ;OUTPUT FIRE STATUS
            EVEN
    LPNN:   MOV.B   DO1,&WKR2
            AND.B   DO2,&WKR2
            AND.B   DO3,&WKR2
    ;       BIS.B   DO4,&WKR2
    ;       BIS.B   DO5,&WKR2
            BIT.B   #040h,&WKR2
            JNZ     CHKIN
            EVEN
    CHK5:   BIT.B   #020h,&WKR2
            JNZ     LAOP         ;low active
            BIT.B   #001h,&RLYON
            JNZ     CLRDO
            JMP     LAOP 
            EVEN
    CHK5ON: BIC.B   #040h,&P1OUT    ;set relay on
            BIS.B   #01h,&RLYON
            JMP     LAOP      ;LOOP BACK IF BIT5 SETTED
            EVEN
    CK5OFF: BIS.B   #040h,&P1OUT    ;Reset relay off         
            EVEN
    CLRDO:  CLR.B   &RLYON     ;CLEAR FLAGS
            JMP     LAOP
            EVEN
    DIOS:    
            JNZ     DOUT          ;FIREED 
           
    FOUT:    
            EVEN
    DOUT:    
            JMP     LAOP
            
    //J2init: NOP
    //        JMP     init
            EVEN
    CHKIN:  BIT.B   #002h,&XMTIN   ;FIRE BIT 5 = P2.1   
            JNZ     CHKYES
            JMP     CHK5
            EVEN
    CHKYES:  
            EVEN
    LPIN:   BIC.B   #F_IN,&DFLAG
            EVEN
            CMP.B   #14,&LASTHI    ;#15
            JNE     LPNXT
            CALL    #SWSR
            EVEN
    LPNXT:   
     
    LP1:    CMP.B   &DO2,&DO1
            JEQ     LP7C
            JMP     LP7B
    LP7A:   CMP.B   &DO3,&DO1
            JEQ     LP7C
            JMP     LP7B
            EVEN
    LP7C:   BIT.B   #020h,&DO1   ;TEST BIT 5 FOR RELAY ON
            JNZ     SETOUT
            JMP     RSTOUT 
            EVEN
    SETOUT: BIC.B   #040h,&P1OUT    ;set relay on P1.6 low active
            BIS.B   #001h,&RLYON 
            JMP     LP7B
            EVEN
    RSTOUT: BIT.B   #001h,&RLYON 
            JNZ     LP7B
            BIS.B   #040h,&P1OUT    ;Reset relay off p1.6 
            EVEN        
    LP7B:   CMP.B   #08h,&BITCNT    ;bitcnt==8 check pooled address  
            JEQ     LP8A
            JMP     LP8B
    LP8A:   MOV.B   &RCVHI,&CADDR   ;CADDR store pooled address
            CMP.B   &ADDR,&CADDR    ;ADDR store parityed device address
            JNE     LPB
    //        MOV.B   &RCVLO,&CADDR
    //        AND.B   #80h,&CADDR
    //        CMP.B   &ADDRL,&CADDR
    //        JNE     LPB
            BIS.B   #F_MAT,&CFLAG
            BIS.B   #F_MAT,&DFLAG 
            
            TST.B   &FLASH
            JZ      LPB
            BIT.B   #03h,&XMTIN      ;if alarm or fault disable pooling flash
            JNZ      LP8M
            BIS.B   #10h,&P1OUT      ;SET P1.4 TO FLASH LINK LEDP1.4=RED
    LP8M:   CLR.B   &FLASH
        
    //        TST.B   &FLASH
    //        JZ      LPB
    //        BIS.B   #10h,&P1OUT      ;SET PB7=P1.6GREEN TO FLASH LINK LEDP1.4=RED
    //        CLR.B   &FLASH
    //       XOR.B   #020h,P2OUT     ;TEST ADDRRESS MATCH FLASH LED P2.5
            
            JMP     LPB
    JJ2init: NOP        
            jmp     J2init
            EVEN
    LP8B:   CMP.B   #16,&BITCNT      ;#17
            JEQ     LPA
            JMP     LPB
            EVEN
    LPA:    INC.B   &FRMCNT
       //     BIS.B   #020h,P2OUT     ;TEST ADDRRESS MATCH FLASH LED P2.5 $$
            CLR.B   &BITCNT
            BIC.B   #F_MAT,&CFLAG
            BIC.B   #F_SYS,&CFLAG
            EVEN
    LPB:     
      
            BIT.B   #F_MAT,&CFLAG
            JNZ     LPC
            //-INV.B   &CIN
            //-MOV.B   &CIN,&XMTIN
            JMP     LP2
            EVEN
    LPC:    BIT.B   #F_MAT,&DFLAG
            JNZ     LP2
            EVEN
            CMP.B   #013,&BITCNT     ;#14
            JNE     LP14
            CALL    #CHKDO
            JMP     LP2
            EVEN
    LP14:   CMP.B   #14,&BITCNT      ;#15
            JNE     LP15
            CALL    #FMTI2
            JMP     LP2
            EVEN
    LP15:   CMP.B   #15,&BITCNT      ;#16
            JNE     LP2
            CALL    #FMTPI
    LP2:    EVEN
            JMP     LAOP
     
    ;
    ;CHKDO USE TO CHECK DO AND FORMAT I1
    ;
            EVEN
    CHKDO:  BIS.B   #F_MAT,&DFLAG
            BIC.B   #F_PAS,&CFLAG
            CLR.B   &CCS
            MOV.B   &RCVHI,&WORK
            BIT.B   #008h,&WORK    ;TEST FIRE BIT 3
            JZ      CK3
            INV.B   &CCS
    CK3:    BIT.B   #010h,&WORK    ;TEST FAULT BIT 4
            JZ      CK4
            INV.B   &CCS
    CK4:    BIT.B   #020h,&WORK    ;TEST RELAY BIT 5
            JZ      CK5
            INV.B   &CCS
    CK5:    BIT.B   #040h,&WORK    ;TEST MANUAL BIT 6
            JZ      CK6
            INV.B   &CCS
    CK6:    BIT.B   #080h,&WORK    ;TEST PARITY BIT 7
            JZ      CK7
            INV.B   &CCS
    CK7:    TST.B   &CCS
            JNZ     CHKA
            INV.B   &WORK
            AND.B   #0F8h,&WORK
            MOV.B   &DO4,&DO5
            MOV.B   &DO3,&DO4
            MOV.B   &DO2,&DO3
            MOV.B   &DO1,&DO2
            MOV.B   &WORK,&DO1
            BIT.B   #008h,&DO1     ;TEST BIT 3 FIRE TEST
            JNZ     CHK9
            JMP     CHKA
    CHK9:   BIS.B   #F_POST,&CFLAG
            BIS.B   #F_PAS,&CFLAG
            BIC.B   #040h,&XMTIN     ;RESET BIT 1 = P2.6
            RET
    CHKA:   BIT.B   #F_POST,&CFLAG
            JZ      CHKA1
            RET
    CHKA1:  BIT.B   #002h,&XMTIN     ;PB5 = P2.1 FOR FIRE STATUS
            JNZ     CHKB
            RET
    CHKB:   BIS.B   #F_POST,&CFLAG
            BIS.B   #F_PAS,&CFLAG
            AND.B   #0EFh,&DO1
            //-TST.B   &RLY_FLAG       ///
            //-JZ      T1NXT
            RET
    T1NXT:  BIS.B   #004h,&P2OUT    ;FIRE LED ON PB6=P2.2
            RET
     
    
    ;
    ;FMTI2 FORMAT I2
    ;
            EVEN
    FMTI2:  BIS.B   #F_MAT,&DFLAG
            BIT.B   #010h,&DO1
            JNZ     FMT9
            JMP     FMTA
    FMT9:   BIS.B   #F_POST,&CFLAG
            BIT.B   #F_PAS,&CFLAG
            JNZ     FM1
            JMP     FM2
    FM1:    BIC.B   #F_PAS,&CFLAG
            JMP     FMTA
    FM2:    BIS.B   #F_PAS,&CFLAG
    FMTA:   BIT.B   #F_POST,&CFLAG
            JZ      FMTA1
            RET
            EVEN
    FMTA1:  BIT.B   #001h,&XMTIN    ;PB0 = P2.0 FOR FAULT STATUS
            JNZ     FM5
            BIT.B   #002h,&XMTIN    ;TEST P2.1 FIRE
            JZ      FM7
            RET
    FM7:    TST.B   &RLY_FLAG
            JNZ      FM7A         
    //        BIC.B   #004h,&P2OUT    ;CLERA PB6=P2.2 LED
            EVEN
    FM7A:   RET
            EVEN
    FM5:    BIS.B   #F_POST,&CFLAG
            TST.B   &RLY_FLAG
            JNZ     FM6
            TST.B   &FAULT
            JZ      FM6
    //         XOR.B   #004h,&P2OUT    ;TOGGLE LED FOR FAULT
            CLR.B   &FAULT
    FM6:    BIT.B   #F_PAS,&CFLAG
            JZ      FM4
    FM3:    BIC.B   #F_PAS,&CFLAG
            RET
    FM4:    BIS.B   #F_PAS,&CFLAG
            RET
    ;
    ;FMTPI FORMAT IP INPUT PARITY
    ;
            EVEN
    FMTPI:  BIS.B   #F_MAT,&DFLAG
            BIT.B   #F_PAS,&CFLAG
            JZ      FMTPI1
            RET
    FMTPI1: BIS.B   #F_POST,&CFLAG
            RET
    ;
    ;Write_Lowest  ;use to write LOWEST Value to SegmentC #01040h
    ;
    WrtLow: nop
            mov      #LOGTBL,R6
            mov      0(R6),&WORKD
            add      2(R6),&WORKD
            add      4(R6),&WORKD
            add      6(R6),&WORKD
            rra      &WORKD
            rra      &WORKD
            mov      &WORKD,&LOWEST
            mov.w    #01040h,R5
            mov.w    #FWKEY+FSSEL0+FN1,&FCTL2
            mov.w    #FWKEY,&FCTL3
            mov.w    #FWKEY+ERASE,&FCTL1
            mov.w    #0,&01040h
    Prog_segC
            mov.w    #FWKEY+WRT,&FCTL1
            mov.w    #FWKEY,&FCTL3
            mov.w    &LOWEST,0(R5)
    //        mov.b    &LOWEST,0(R5)
    //        mov.b    &LOWEST1,1(R5)
            mov.w    #FWKEY+LOCK,&FCTL3
            ret                 
    ;
    ;P1ISR P1.0  CLOCK SIGNAL INTERRPT SERVICE ROUTINE 
    ; 
            EVEN
    P1ISR:  BIC.B   #020h,&P1IFG    ;CLEAR INT FLAG P1.5 CLK
    
    //        XOR.B   #020h,P2OUT     ;TEST ADDRRESS MATCH FLASH LED P2.5 
            
            BIT.B   #020h,&P1IES    ; 1= H2L 0= L2H
            JZ      CLKL2H
    CLKH2L: BIC.B   #020h,&P1IES     ;CHANGE TO L2H  *****
            BIT.B   #F_POST,&CFLAG
            JZ      CLKH3
            BIC.B   #02h,&P1OUT   ;P1.1 = PB1 DATA LOW ACTIVE
    CLKH3:  BIC.B   #F_BIT,&CFLAG
    //        BIC     #LPM3,0(SP)
            RETI
    ;
    ;CLKL2H CLOCK P1.0 = PB4 Lo>Hi
    ;
            EVEN
    CLKL2H: BIS.B   #002h,&P1OUT   ;P1.1 = PB1 RESET DATA OUTPUT
    //        TST.B   &RLY_FLAG
    //        JNZ     T3NXT
            BIT.B    #03h,&XMTIN
            JNZ      T3NXT          ;if fire or fault don't clear red led
            BIC.B   #010h,&P1OUT   ;RESET P1.6=GREEN FLASH P1.4=RED
    T3NXT:  BIS.B   #020h,&P1IES   ;SET EDGE H2L  *****
            BIS.B   #F_IN,&DFLAG
            CLRC
            BIT.B   #F_IN,&CFLAG
            JZ      CLKL4
            INC.B     &HICNT
            SETC
    CLKL4:  RRC.B   &RCVHI       ;ROTATE DATA BIT INTO RCV BUFFER
            RRC.B   &RCVLO       ;DITTO
            INC.B   &BITCNT      ;ONE BIT END
            BIS.B   #F_IN,&CFLAG ;DATA NORMAL HIGH
            BIS.B   #F_BIT,&CFLAG  ;ONE BIT COMPLETED
            BIC.B   #F_POST,&CFLAG
            BIC.B   #F_MAT,&DFLAG
     //       BIC     #LPM3,0(SP)
            RETI
            
            
    ;
    ;DATH2L FOR DATA Hi>Lo P2.4 = PB2
    ; 
            EVEN
    P2ISR:  BIC.B   #F_IN,&CFLAG
            MOV.B   &HICNT,&LASTHI
            CLR.B   &HICNT
            BIC.B   #001h,&P2IFG    ;P2.0 DATA
     
     //       XOR.B   #020h,P2OUT     ;TEST ADDRRESS MATCH FLASH LED P2.5
     //       BIC     #LPM3,0(SP)
    P2END:  RETI  
    
    ;
    ;SYNC DATA CHECKING
    ;
            EVEN
    SWSR:   CMP.B   #07Fh,&RCVHI
            JEQ     SW1
            RET
    SW1:    CMP.B   #0FEh,&RCVLO  ;14 bits high
            JEQ     SW2
            RET
    SW2:    CLR.B   &FRMCNT
            CLR.B   &BITCNT
            CLR.B   &LASTHI
            CLR.B   &HICNT
            CLR.B   &RCVHI
            CLR.B   &RCVLO
            
       //     XOR.B   #020h,P2OUT     ;TEST ADDRRESS MATCH FLASH LED P2.5
            
            RET
            
            EVEN
    WDISR:  NOP
                     
            BIC.B   #WDTIFG,&IFG1
            JMP     JJ2init 
            RETI
            EVEN
            
    TMISR:  NOP
            BIC     #01h,&TACTL     ;CLEAR TAIFG
            EVEN
            CMP     #190,&CNT4       //200~160 ON
            JGE     TMN1            ;LED ON
            CMP     #150,&CNT4      //160~120 OFF
            JGE     TMN0            ;Keep LED Off
            CMP     #140,&CNT4       //120~80  ON
            JGE     TMN5            ;LED OFF  
            BIC.B   #10h,&P1OUT    ;clear LED
             
            JMP     TMN2
    TMN5:   BIT.B   #02h,&XMTIN
            JZ     TMN2
            BIS.B   #10h,&P1OUT    ;Lit LED
            JMP     TMN2
    TMN0:   BIC.B   #10h,&P1OUT    ;Clear  LED   
            JMP     TMN2
    TMN1:   BIT.B   #03h,&XMTIN
            JZ      TMN2
            BIS.B   #10h,&P1OUT    ;Lit LED         
            EVEN
    TMN2:   DEC.B   &TMCNT
            JNZ     TMRTN        
    //TMNOR:  DEC.B   &TMCNT
    //        JNZ     TMRTN
            EVEN
    TMZERO: MOV.B   #150,&TMCNT
    //        MOV.B   #0Fh,&FLASH
            MOV.B   #0Fh,&FAULT
    //        DEC.B   &SENCNT
    //        JNZ     TMRTN
    //        MOV.B   &SENTM,&SENCNT
    //        MOV.B   #77h,&SENFLAG
            DEC.B   &FCNT1
            JNZ     TMRTNB
            MOV.B   #0Fh,&FLASH
            MOV.B   #5,&FCNT1
    TMRTNB: INC.B   &TSTCNT
            cmp.b   #1,&TSTCNT
            jne     TMRTN
            bic.b   #08h,&P1OUT             ;op power on low active 
    ;TEST TIMER
    //         XOR.B   #10h,&P1OUT    ;toggle RED LED for testing
            EVEN
    TMRTN:  NOP
            DEC       &CNT4
            JNZ       TMRTN2
            MOV       #200,&CNT4
              
             BIT.B   #03h,&XMTIN
             JZ      TMRTN2
             BIS.B   #10h,&P1OUT    ;Lit LED
    TMRTN2: NOP        
            RETI
    //        
    ADC10U: NOP
            CLR.B   &ADCFLAG
    //        BIC     #LPM0,0(SP)
            RETI
     ;
    ;WORKC = WORKA / WORKB
    ;
            EVEN
    DIVID2: NOP
            TST.B  &ActFlag
            JZ     DIVNXT
            RET
            EVEN
    DIVNXT: CLR     &WORKC
            MOV     &STDBASE,&WORKA
            MOV     &LOWEST,&WORKB
            MOV.B   #16,DOCNT16
    DOLOOP: CLRC
            RLC     &WORKA
            RLC     &WORKC
            CMP     &WORKB,&WORKC
            JGE     DLOP1
            CLRC
            JMP     DLOP2
    DLOP1:  SUB     &WORKB,&WORKC
            SETC
    DLOP2:  RLC     &WORKD          ;Q  
            DEC.B   &DOCNT16
            JNZ     DOLOOP
            MOV.W   &WORKD,&ADJ
            RET
    ;
    ;MULTADJ  RMKR3 * ADJ / 64
    ;        
             EVEN
    MULTADJ: NOP
             MOV.W  &SMKR3,&WORKA
             MOV.W  &ADJ,&WORKB
             CLR.W  &WORKC
             CLR.W  &WORKD
             CLR.W  &WORKE
             MOV.B  &8,&DOCNT16
    MLOOP:   RRC.W  &WORKA         
             JNC    MLOP1
             CLRC
             ADD.W  &WORKB,&WORKD
             ADDC.W &WORKC,&WORKE
    MLOP1:   CLRC
             RLC.W  &WORKB
             RLC.W  &WORKC
             DEC.B  &DOCNT16
             JNZ    MLOOP
             MOV.B  #6,&DOCNT16
    MD64:    CLRC
              RRC.W  &WORKE
              RRC.W  &WORKD
             DEC.B  &DOCNT16
             JNZ    MD64
             AND.W   #07FFh,&WORKD     ;2025/11/27
             MOV.W  &WORKD,&SMKR3
             RET
    //
    //Vectors
    //
            ORG     0FFE0h
            DC16    init            ; set reset vector to 'init' label
            DC16    init            ; E2 set reset vector to 'init' label
            ORG     0FFE4h
            DC16    P1ISR           ;PORT 1 ISR
            ORG     0FFE6h
            DC16    P2ISR           ;PORT 2 ISR
            DC16    init        ;E8
            DC16    ADC10U      ;EA
            DC16    init        ;EC
            DC16    init        ;EE
            ORG     0FFF0h
            DC16    TMISR       ;F0  TIMER 2
            DC16    init        ;F2  TIMER 2
            
            ORG     0FFF4h          
            DC16    WDISR       ;WATCH DOG ISR
            DC16    init        ;F6  COMP A+
            DC16    init        ;F8
            DC16    init        ;FA
            DC16    init        ;FC  NMI  
            
            ORG     0FFFEh
            DC16    init            ; set reset vector to 'init' label
            
                                    
            END

  • Dear All:

       Main.asm and ***.s43 are same.

       INPUT PORT interupt response time are different, whitch make the IAR  *.D43 works correctly, and CCS ***.out not function correctly.

       Could comeone tell me how to improve the INPUT PORT interrupt response time ?

        Thanks  a lot to all friends !

        Best regards;

      Marshall Wu 2026/03/20

  • Hello Marshall,

    In fact, the CPU response speed to interrupt is decided by hardware. I don't think it will be different when the two project files have the same hardware configuration (such as main frequency). Otherwise, the response speed you mean is the time from interrupt trigger signal occurs to the interrupt handling action occurs, if so, maybe the different compiler has different compile action to the same one assembly file.

    You can try to generate a very simply project, just keep the interrupt handler code, and in the handler, directly toggle one GPIO. and test whether the GPIO toggle has different speed when in CCS and IAR. The easier project, will be more helpful, if we need software engineer to look into this issue,

    best Regards,

    Janz Bai