Other Parts Discussed in Thread: TMS320VC5505, TMS320C5505
Hi everyone,
I am currently working on a project that uses a TMS320VC5505 DSP board. I've built up my project using examples that were given on the google code website and on the CD, and so far everything has worked.
As I needed a UART example, I installed the CSL and intended to try out the examples there, however everytime I try run any of the examples I get the same error code:
This project was created for a device-variant that is not currently recognized: TMS320C55XX.TMS320C5505. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants. CSL_UART_pollExample project 1328540016920 1187
CCS is version : 4.0.0.16000 and when I click update it says it's the lastest version (although I have a feeling it is not).
The code still builds and compiles it's only when I try to connect to the target it fails.Some help please :D I've spent a few days trying to debug this problem and my collegue is as confused as I am.
Target Configuration:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS100 USB Emulator_0">
<instance XML_version="1.2" desc="Texas Instruments XDS100 USB Emulator_0" href="connections\TIXDS100usb_Connection.xml" id="Texas Instruments XDS100 USB Emulator_0" xml="TIXDS100usb_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS100 USB Emulator_0">
<instance XML_version="1.2" href="drivers\tixds100c55x.xml" id="drivers" xml="tixds100c55x.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="USBSTK5505_0" href="boards\usbstk5505.xml" id="USBSTK5505_0" xml="usbstk5505.xml" xmlpath="boards"/>
</platform>
</connection>
</configuration>
</configurations>
Cheers
Daniel.