I am just coming back to using TI dsp after 6yrs. I can remember how to begin running or modifying existing projects.
I decided to follow a Quickstart_Reamme pdf document called "2803x C/C++ Header Files and Peripheral Examples Quick Start".
Below is the error I got trying to run one of the example project. I believe I have version 4 of the code composer, how can this problem be resolved?
Error
Exception occured during launch
Reason:
Program files does not exist.
Severity and Description Path Resource Location Creation Time Id
This project was created using a version of Code Generation tools that is not currently installed: 5.2.1 [C2000]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions. Example_2803xCpuTimer properties 1328556019911 578