This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3105: LIN communication establishment - How can be done

Part Number: MSPM0G3105

I am using the MSPM03105 Launch Pad and I would like to test the LIN communication. Seems there is no LIN Transceiver and how could establish the LIN communication here.

  • Hi Desingh,
    You will need a transceiver to run our LIN examples. Alternatively, maybe by using jumper cables and making the connections into one single line/bus through our open drain pins that are capable of handling 5V, could be an alternative to not using a LIN transceiver (I would try this and see if it works. Otherwise, the recommended way is using a transceiver).
    Best Regards,
    Diego Abad