This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO-THEIA: PROJECT ENVIRONMENT SETTING FOR MULTI CORE

Part Number: CCSTUDIO-THEIA

I am trying to set a project environment for multicore. i am using TM320F28388D controller and it has 3 cores. in which i want to make use of all the three cores. so i need a support on how to setup the environment for multicore. is it like need to create seperate projects for all the three cores or in a single project we can setup the environment for multicore. during new project setup i noticed in the project wizard page in the project file space i can see few options which says Driverlib Empty CM Example CCS Project and Driverlib Empty CPU1 Example CCS Project  we have to follow these things to setup for multicore thing.