Part Number: AM261X-MCAL-SDK
Hi,
I am trying to debug example project on the AM261x LP hardware. When I start debug project, I got below error. I tried to power-cycle the board as suggested but I still got same errors. I also tried to set lower TCLK (100kHz) but I still got same errors. Please help how I can fix this problem.
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.4.0.3835)