This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: Unable to download Hercules lwIP example (RM57L843) from TI cgit repository

Part Number: RM57L843

Dear TI Support Team,

I am currently working with the RM57L843 Hercules microcontroller and need to access the lwIP example project available in the Hercules Examples repository.

I have attempted multiple methods to access and download the repository from official TI sources, but without success.

Repository links used:

* https://git.ti.com/cgit/hercules_examples/hercules_examples/
* https://git.ti.com/cgit/hercules_examples/hercules_examples/tree/Application/LwIP
* https://git.ti.com/cgit/hercules_examples/hercules_examples/tree/Application/LwIP/v00.04.00

Attempted download methods:

* Browser access via cgit interface (no visible or functional snapshot option)
* Direct snapshot download attempts:

  * https://git.ti.com/cgit/hercules_examples/hercules_examples/snapshot/hercules_examples-master.zip
  * https://git.ti.com/cgit/hercules_examples/hercules_examples/snapshot/hercules_examples-master.tar.gz
* Git clone attempts:

  * git clone https://git.ti.com/hercules_examples/hercules_examples.git → HTTP 403 error
  * git clone git://git.ti.com/hercules_examples/hercules_examples.git → blocked or not accessible

Observed issues:

* “Unsupported snapshot format” when attempting direct downloads
* HTTP 403 error when cloning via HTTPS
* No working download option in the cgit interface

Due to these issues, I am unable to obtain the lwIP example located under:
Application/LwIP/v00.04.00/RM57x

Could you please provide:

1. A direct and functional download link (ZIP or other format) for the Hercules Examples package, specifically including the lwIP example for RM57
2. Alternatively, a recommended official method to access or download these examples

This example is critical for implementing TCP/IP communication on the RM57 platform for an industrial data acquisition application.

Thank you for your support.

Best regards,
Martin Valencia
Senior Industrial Applications Engineer