Part Number: TMS320F28P650SK
Hello guys, another bloody problem....
The iMac that CCS20.5.0 is installed on is not connected to the web due to hi security risk.
When I build the ASM program CCS20.5.0 tries to connect to a TI server for some reason and it just waits until I press the reset button and then CCS20.5.0 restarts. Grrrrrrr.
It should NOT have to contact any webserver to build any programs, everything CCS20.5.0 needs should already be installed locally when CCS20.5.0 was installed.
NO, sorry but this iMac is strictly no internet access period.
CCS20.4.1 worked fine even with NO internet access but CCS20.5.0 does not.
How do I fix this?
Peter