This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

My linker created a --HOLE-- (fill = 0)



 I have been trying to compile an operational version of an example project.

But there is a problem...

The compiler appears to "compiles" NOP instructions into "--HOLE--" locations that are created when the linker fails to find the source code from the library.

> I expected that the compiler would stop and that the code composer would show an error for the missing link.

map file output - extract:
SECTION ALLOCATION MAP

output attributes/
section page origin length input sections
-------- ---- ---------- ---------- ----------------
.pinit 0 003f4000 00000000 UNINITIALIZED

phyRamFuncs
* 0 003e8000 000013c5 RUN ADDR = 00008c00
003e8000 00000900 phy_lin_afe031_f2806x.lib : phy_cfft16i_vcu.obj (phyRamFuncs)
003e8900 000001d3 : phy_cfft16c_256p_vcu.obj (phyRamFuncs)
003e8ad3 00000001 --HOLE-- [fill = 0]
003e8ad4 0000018f : phy_cfft16c_128p_vcu.obj (phyRamFuncs)
003e8c63 00000001 --HOLE-- [fill = 0]
003e8c64 00000185 : phy_eqz.obj (phyRamFuncs)
When I look at the disassembler and step my way through the code, I find a link to the missing file
T:/csa_group_emeter/dspsrdc_csa/emeter/dsp_c28x/src/fft/phy_cfft16i_vcu.asm:49:66

Disassembly extract:

0x3EF729:   8F4096D4    MOVL         XAR5, #0x0096d4
0x3EF72B: A094 MOVL *+XAR4[AR0], XAR5
0x3EF72C: 76408C00 LCR $T:/csa_group_emeter/dspsrdc_csa/emeter/dsp_c28x/src/fft/phy_cfft16i_vcu.asm:49:66$
0x3EF72E: 0006 LRETR
InitPeripheralClocks:
0x3EF72F: 7622 EALLOW

> Is this normal behaviour?
  • The linker creates holes to satisfy alignment requirements.  In this case, it is creating holes after the phyRamFuncs sections of object files "phy_cfft16c_256p_vcu.obj" and "phy_cfft16c_128p_vcu.obj" because those sections have an odd number of bytes and presumably even alignment.  If you use ofd2000 on each of those two object files and look at the section phyRamFuncs, it should show that they have even alignment and odd size.  None of this so far is a bug

    Which symbol used in phy_cfft16c_256p_vcu.obj should the linker have found in the library?  Please change your linker options to generate a map file, and post that here.  It should show whether or not the linker found that symbol.

    [Edit: I should have been more precise.  There is a hole after phy_cfft16c_256p_vcu.obj because phy_cfft16c_128p_vcu.obj has alignment 2, and there is a hole after phy_cfft16c_128p_vcu.obj because phy_eqz.obj has alignment 2. --Archaeologist]

  • I have a library file that includes the command LCR 0x369ad8, which sends to the code to unused code space. 

    The pre-compiled library function TF_256P_CFFT is used by the library function "PHY_txInit()" to initialise the tx section of the code.

     Under PHY_txInit:, there is a call to the function PHY_rifft16_512p_init: and this calls PHY_cfft16_init, and this crashes the program.

    At the library location (TF_256P_CFFT + 0x1c), which is used under the 

    0x008C22:   EB7F        SUBR         *-SP[63], AH
    0x008C23: 5DA6 MOVZ AR5, @AR6
    0x008C24: 76769AD8 LCR 0x369ad8 <--- This command jumps the program to...

    util_block_short_offset + 0x35fb16
    0x369AD8:   ????????
    0x369AD9: ????????
    0x369ADA: ????????
    This code is from the file... T:csa_group_emeter/dspsrdc_csa/emeter/dsp_c28x/src/fft/phy_cfft16i_vcu.asm that has been compiled into the library file.
    
    
    The initialisation function is described in the header file "phy_tx.h" by fum and updated by S. Yim in 2009.
    It is part of the PrimeDevelopmentPackageV6005.
    
    
    Do you have a fix?
  • I am not at all familiar with that library.  I think we will need someone who is familiar with it to enter this discussion.

    Your symptom is that the program has a branch to an apparently bogus address.  I cannot guess why that might be so; I would need a test case to pursue this issue.